+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Temperature inversion is a meteorological phenomenon involving an inversion of the normal atmospheric temperature gradient in which the temperature, instead of decreasing with increasing altitude, increases in a particular layer of air. Under typical tropospheric conditions, the temperature decreases at a rate of about 6.5°C for every kilometre of altitude, whereas in the case of an inversion, an increase in temperature with altitude is observed in a layer limited to tens or hundreds of metres.
Others physical processes may be involved in the mechanism of inversion formation, including the radiation of heat from the Earth's surface on cloudless, cool nights, the influx of warmer air over the cooler Earth's surface, or the compression of air as a result of subsidence in high-pressure systems. Under conditions of lower atmospheric inversion, the vertical exchange of air masses is reduced, leading to the accumulation of pollutants, aerosols and moisture near the ground surface.
Temperature inversion plays an important role in shaping local weather conditions and air quality, especially in urban areas and mountain valleys, where it can cause significant deterioration in visibility and an increase in the concentration of harmful substances in the atmosphere. In environmental engineering and meteorology, numerical models are used to predict inversion conditions, which is important for the design of natural ventilation systems, urban planning and environmental impact assessments of investments.
The phenomenon of temperature inversion also affects the propagation of electromagnetic waves, including radio waves and radar waves, by changing refraction atmospheric, which can lead to increased signal coverage or interference effects. In the context of climatic variability, inversions can affect the energy balance of the earth's surface and atmospheric dynamics, particularly in polar regions where there are prolonged inversions associated with ice cover and limited solar heating.
In research, the analysis of temperature inversions is an important element in monitoring urban heat island effects, radiation haze formation processes and atmospheric boundary layer dynamics, which is of direct relevance for modelling pollutant transport and predicting extreme weather events.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.