+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Compactron - definition

The Compactron is a type of electron tube built in a miniaturised form, mainly intended for use in high-density electronic instrumentation such as military, aerospace, computer equipment and professional measurement and telecommunications systems. Developed in the mid-20th century as a response to the need for miniaturisation of vacuum components, compactrons combined several active structures, e.g. a triode, pentode or a diode, in a single glass bulb, thus significantly reducing the number of components and simplifying instrumentation circuits.

A characteristic feature of compactrons was the integration of several functional circuits in a single enclosure, while maintaining a hermetic vacuum seal. The internal components were mounted coaxially or concentrically, and their electrodes were brought out through common or separate base pins. This resulted in better electrical stability, reduced parasitic capacitances and reduced signal loss at high frequencies.

Compactrons found widespread use in the 1950s and 1960s, especially in analogue technology, before being displaced by transistors and integrated circuits. They allowed more complex functions to be performed in a limited space, while reducing manufacturing costs and simplifying assembly. They were often used in amplifier circuits, generators, frequency mixers, detectors and as logic elements in early generation digital systems.

Due to their design, compactrons were characterised by favourable thermal performance, good mechanical resistance and low noise emissions compared to classical electron tubes. Today, they are an object of interest for collectors and specialists involved in the preservation and restoration of vintage electronic devices, especially audio equipment and vintage Measuring Instruments.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO