+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
Microelectronics is a branch of electronics that deals with the design, manufacture and testing of very small electronic systems, with components on the order of micrometres or nanometres in size. It represents an evolution of traditional electronics towards miniaturisation and integration of electronic functions, making it possible to create complex systems on a small area of silicon substrate. Microelectronics is the basis of modern digital and analogue technologies, used in computers, mobile devices, control systems, medical apparatus, and the automotive and aerospace industries, among others.
The foundation of microelectronics is Semiconductors, mainly silicon, from which integrated circuits (ICs - Integrated Circuits) are created. Microelectronic technologies include lithography, chemical etching, ion implantation and the deposition of dielectric and metallic layers under vacuum conditions. These processes enable Transistors, Resistors, Capacitors and other components to be formed within a single chip.
Developments in microelectronics are enabling increased component packing density, resulting in higher performance and energy-efficient devices. Central to this is Moore's Law, which for Decades described the trend of doubling the number of Transistors on an Integrated circuits every two years or so. Modern microelectronics also includes design at the level of logic circuits and digital systems, using hardware description languages such as VHDL or Verilog.
Also associated with microelectronics is so-called nanoelectronics, which continues the drive towards miniaturisation below the limits of conventional optical lithography. This limit poses both technological and physical challenges related to quantum and thermal effects at the level of single atomic structures.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.