+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Inductor (choke) - definition

Choke is a passive component of electrical and electronic circuits whose primary property is inductance—the ability to store energy in a magnetic field generated by the flowing current. It consists of a coil of wire wound around a magnetic or air core, and its operation is based on opposing sudden changes in electric current. A choke primarily resists alternating currents while offering much less impedance to direct currents, making it an effective filter in power supply and signal applications.

In alternating current circuits, a choke limits current fluctuations and suppresses electromagnetic interference and harmonics. Thanks to its ability to "smooth" signals, it is used in switching converters, power supplies, filtering circuits, and interference suppression systems. Depending on its construction and core material, chokes can operate over a wide range of frequencies and power levels, allowing their use in both microelectronics and power installations.

In lighting technology, chokes are also used in discharge lamp circuits, where they act as current limiters and ignition components. The operational characteristics of a choke depend on its inductance, self-resistance, core type, and coil geometry. These parameters affect its noise suppression efficiency, energy performance, and resistance to varying operating conditions. Chokes are essential components in the design of reliable and stable electronic systems, especially in environments exposed to high-frequency impulses and interference.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO