+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

MOSFET - definition

MOSFET (Metal-Oxide-Semiconductor Field-Effect Transistor) is a semiconductor field-effect transistor in which the current flow between two electrodes - the source and the drain - is controlled by a voltage applied to the gate electrode. This gate is separated from the semiconductor channel by a thin insulating layer of metal oxide. This structure enables contactless and highly efficient control of channel conductivity, making the MOSFET one of the most widely used components in electronic and microprocessor circuits.

The fundamental structure of a MOSFET is based on the MOS configuration, where the gate made of a conductive material (e.g., polysilicon or metal) is located above a thin dielectric layer, typically silicon dioxide, which in turn lies above the semiconductor substrate. Applying an appropriate voltage to the gate induces a conductive channel between the source and drain, the properties of which depend on the transistor type (n-channel or p-channel). The current flow is governed entirely by the electric field, without any charge transfer through the gate itself.

MOSFETs are characterized by very high input impedance, low static power consumption, and high switching speed, making them indispensable in digital circuits such as logic gates, registers, and processors. In analog applications, they are used as amplifiers or switches, while in power electronics they function as control elements in converters, voltage regulators, and inverters. In CMOS technology—dominant in modern integrated circuits—complementary pairs of n-type and p-type MOSFETs are used to reduce energy losses and improve operational reliability.

The advancement of MOSFET technology has led to the development of various structural variants, including depletion-mode devices, trench-type transistors, planar designs, and multi-gate architectures. Thanks to their miniaturization capabilities and integration potential within large silicon structures, MOSFETs are the foundational building blocks of modern electronic systems, forming the core of contemporary microelectronics, automation, and embedded systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO