+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Android is an open-source operating system based on the Linux kernel, designed for mobile devices, such as smartphones, tablets, smart watches and televisions. It was created by Android Inc., and subsequently acquired and developed by Google, which provides continuous support and functional and security updates. The system features a modular architecture, it is modular in architecture and adaptable to different classes of electronic equipment.
Android uses interfaces based on tactile user experience, supporting gestures such as dragging, tapping or pinching. Applications running on this system are mainly written in the following languages Java and Kotlin, and their code is executed by the Android Runtime Virtual Machine (ART). This environment provides memory management, application security and support for multiple threads. The system also includes its own resource manager, inter-process communication mechanisms and a set of multimedia libraries.
The Android platform supports a wide range of hardware and software components, including various screen resolutions, communication interfaces (Wi-Fi, Bluetooth, NFC), location GPS and Environmental Sensors. Its flexibility and accessibility have made it, has made it the most popular mobile operating system in the world, used by many manufacturers in a wide variety of devices.
Google releases the base version of Android as an AOSP project (Android Open Source Project), while the commercial version, integrated with Google Mobile Services (GMS), includes, among other things, the Play Store, Google Maps and synchronisation with a Google Account. The system is regularly developed, and subsequent versions introduce new features, security fixes and improvements in performance and power management.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.