+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Bias - definition of

Bias is a technical term with a varied meaning, depending on the field of science and technology, in which it is used. In general, it refers to a systematic deviation, distortion or shift in value, which may affect the accuracy, the objectivity or neutrality of the measurement process, algorithm or system.

In electronics, bias refers to the voltage or current of polarisation, used to set appropriate operating conditions for semiconductor components, such as Transistors or Diodes. Proper selection of the bias value allows proper conduction of current and ensures linearity or amplification of the signal. Lack of correct bias can result in signal distortion or incorrect circuit operation.

In statistics and data analysis bias refers to a systematic estimation error, which causes, that the expected value of an estimator differs from the actual value of the parameter. This type of bias may result from faulty sampling, incorrect analysis methodology or external confounding factors.

In the context of artificial intelligence i machine learning bias can refer to both a component of the model's decision function (e.g. as an added value in the neurons of an artificial network), as well as to biases in the training data, that lead to inequalities or undesirable patterns in the performance of the algorithm. Bias in this view is the subject of research into algorithmic ethics and the fairness of decision models.

In each of these areas, bias affects the interpretation of the results of the, operation of equipment or the quality of decisions based on the data being processed, therefore, its identification and control is an important part of the design and analysis process.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO