+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Stepping characteristics is a way of describing the response of a dynamic system to a unit-step forcing, i.e. a sudden change in the input signal from zero to a constant value. Analysing this type of response allows us to determine how a system responds to sudden perturbations or changes in operating conditions. It is one of the basic tools in systems engineering Automation, electronics and control theory.
In practice, spike characteristics are represented as a graph of the output signal as a function of time after a spike has been applied. Its shape depends on the dynamic properties of the object under test, such as inertia, damping, delay or the presence of energy storage elements. In first-order systems, the step response takes the form of an exponential ramp-up, while in higher-order systems oscillations, overshoots or longer settling times may occur.
Step characteristics are important for both analogue and digital systems, and their analysis allows for the assessment of stability, speed of response and quality of control. In system identification methods, they allow the parameters of a mathematical model of an object to be estimated. In Automation, they are often used to select the settings of regulators such as PID, where the spike response plays a key role in the tuning process.
The characteristic is also used in the diagnostics of Instrumentation and mechatronic systems, as any deviation from the predicted response can indicate damage or changes in the parameters of system components. In digital systems, it is analysed from sampled data, which requires the use of numerical tools and smoothing filters to correctly interpret the results.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.