+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Knock sensor is a component of an internal combustion engine control system, responsible for the detection of undesirable detonation combustion phenomena in the cylinder chamber, known as knocking combustion. Its operation is based on the analysis of vibrations generated by rapid changes in pressure, generated by premature auto-ignition initiation of the fuel-air mixture-air mixture, which causes local high-frequency shock waves frequency.
The sensor design is based on a piezoelectric or resistive sensing element, capable of converting the mechanical energy of vibrations into an electrical signal of amplitude proportional to the intensity of knocking. The piezoelectric element generates voltage under the influence of mechanical deformation, which enables the precise recording of signals with frequencies characteristic of knocking combustion, usually in the range of a few kHz to several kHz.
The sensor is mounted directly on the engine block, usually close to the cylinder system, to ensure optimum transmission of mechanical vibrations. Its output signal is sent to the drive unit controller (ECU), which, on the basis of algorithms for signal processing algorithms analyses the vibration characteristics, distinguishing knocking combustion from standard engine vibrations and other mechanical disturbances. In response to detecting a detonation phenomenon, the ECU corrects the ignition advance angle, delaying the initiation of the fuel-air-in response to detonation, the ECU corrects the ignition timing, delaying the initiation of the fuel-air mixture in order to eliminate knocking and protect the-crank system components from damage.
Modern knock sensors use filtering technology and digital signal analysis, which increases the selectivity of detection and allows real-time adaptive adjustment of engine operating parameters. The use of DSP (Digital Signal Processing) systems allows dynamic adjustment of the sensitivity threshold depending on the load and operating temperature of the engine unit.
The high precision of the knock sensor is key to optimising engine performance, enabling the use of more advanced ignition control strategies and reducing harmful exhaust emissions. Its integration with adaptive combustion control systems allows the efficient use of fuels with varying octane counts and provides protection against premature wear of mechanical drive unit components.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.