+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Photo cell - definition

A Photocell is a semiconductor device that converts radiant energy electromagnetic energy, most often sunlight, directly into electrical energy through the photovoltaic phenomenon. Its principle of operation is based on the generation of electron-hole pairs in a semiconductor material under the influence of the absorption of photons with an energy greater than the energy gap. The resulting charge carriers are then separated by the internal field present in the p-n junction, leading to the creation of an electrical voltage and allowing current to flow in the external circuit.

Silicon - both monocrystalline and polycrystalline - is the most commonly used material in the manufacture of photovoltaic cells due to its good conversion efficiency, stability and technological availability. In addition to traditional silicon structures, thin-film photovoltaic cells based on compounds such as CdTe, CIGS or perovskites are also being developed, offering potentially lower production costs and greater application flexibility.

The performance characteristics of a photovoltaic cell depend on parameters such as open-circuit voltage, short-circuit current, maximum power and energy conversion efficiency. This efficiency determines how much of the incident light energy is converted into electrical energy and depends on, among other things, material quality, cell design and lighting conditions. To increase the efficiency of photovoltaic systems, photovoltaic cells are combined into modules and panels, which can be integrated into the energy infrastructure or operate autonomously in off-grid installations.

Photo cells are a fundamental component of photovoltaic technology, playing a key role in the generation of renewable energy. They are used in solar power plants, emergency power systems, portable devices, as well as in specialised applications such as satellites, environmental sensors or powering devices IoT. The development of this technology is focused on increasing efficiency, lowering manufacturing costs and improving durability and integration into the environment.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO