+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The clamp meter is a measuring instrument used for the non-contact measurement of electric current in conductors, without breaking the circuit. Its characteristic feature is the presence of open pincers (jaws) that encompass the conductor, forming a closed magnetic core. From this, using the principle of electromagnetic induction or the Hall effect, the meter records the value of the current flowing.
In the versions for alternating current (AC), the operation of the meter is based on the measurement of the alternating magnetic field generated by the flowing current. The resulting magnetic flux induces a voltage in the secondary winding of the clamps, proportional to the measured current. Modern models capable of measuring direct current (DC) use Hall Sensors, which detect the intensity of the magnetic field and convert it into an electrical signal.
The clamp meter can act as a universal multimeter, also enabling the measurement of voltage, resistance, frequency, capacitance and circuit continuity testing. Its applications include diagnostics of electrical installations, industrial equipment, power systems and building infrastructure. It is particularly useful for measuring high currents or in situations where direct connection to a circuit would be dangerous or technically difficult.
Industrial versions of clamp meters are often equipped with data logging functions, measurement of inrush currents, a power quality analyser or digital interfaces for integration into SCADA and BMS systems. High precision, noise immunity and ergonomic design make the clamp meter an essential tool for electricians, service technicians and maintenance specialists.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.