+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Octave - definition

An Octave is a concept used in acoustics, music and signal analysis, defining a frequency interval in which one frequency is exactly twice the frequency of another. The octave is a fundamental structural module in music systems based on tempered and natural scales, but also in acoustic engineering, where it is used in the spectral analysis of signals and the design of sound reinforcement systems.

In the context of technical analysis, particularly in the field of sound and vibration engineering, the concepts of octave bands and octave thirds are used, which allow a logarithmic division of the frequency range to better interpret the acoustic characteristics of systems or environments. Characteristics in octave bands are useful in assessing the frequency response of rooms, the effectiveness of damping noise or in measuring the acoustic emissions of equipment.

In musical instruments, the octave is also physically important, as it is related to the length of the string, the volume of the resonator or other physical parameters that determine the pitch. In electronic systems, such as active filters or digital signal processing systems, the octave is the reference unit for the design of frequency response characteristics, especially where there is a need for logarithmic frequency scaling.

In wave and dynamical systems theory, the octave plays a key role in describing the behaviour of resonant structures and in modelling phenomena where frequency variation on a logarithmic scale better reflects the perceptual and physical properties of the system under study than a linear scale.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO