+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
PLD (Programmable Logic Device) is a category of digital integrated circuits whose logic functionality can be defined by the user after manufacture. These circuits contain matrices of logic gates and interconnects that can be programmed to perform specific logic functions such as combinational operations, sequential operations, control circuits or protocol conversion. PLDs provide a flexible solution in the design of digital systems, enabling the rapid implementation of complex functions without the need to design specialised circuits (ASICs).
The basic PLD architecture is based on a grid of logical cells or blocks, which can be connected by programmable paths. The programming of the circuit involves defining the configuration of these blocks and their interconnections, which is done using hardware description languages (HDL) such as VHDL or Verilog, and then implemented using specialised software tools.
Others include different classes of PLDs, including PAL (Programmable Array Logic), GAL (Generic Array Logic), CPLD (Complex PLD) and FPGA (Field-Programmable Gate Array). The different types differ in the number of logic resources available, programming method, performance and level of integration. CPLDs offer moderate complexity and good latency predictability, while FPGAs enable the implementation of very complex digital systems, including multi-core processors and systems SoC.
PLDs are used in a wide range of fields - from digital circuit prototyping, consumer, industrial and automotive electronics to aerospace, military and medical systems. Their advantage is the ability to update hardware functionality after deployment, which supports flexible design, rapid patching and adaptation of devices to changing functional requirements and standards. Depending on the technology, PLDs can be one-time programmable (OTP), electrically erasable (EEPROM/Flash) or dynamically reconfigurable.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.