+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Dielectric polarisation - definition

Dielectric polarisation is a physical phenomenon involving the ordering of electrical charges within a dielectric material under the influence of an external electric field. As a result of this field, the molecules or atoms of the material undergo electrical deformation, leading to a shift of the centre of positive charge relative to the centre of negative charge. The effect of this shift is to create microscopic dipole moments, which add up to form the macroscopic polarisation of the material.

The polarisation process does not involve the flow of free charges, but rather their displacement over very small distances in the atomic or molecular structure. Others distinguish between different polarisation mechanisms, depending on the structure of the material and the type of interaction: electron polarisation, associated with the displacement of electron clouds; ionic polarisation, resulting from the displacement of ions in crystal lattices; and orientational polarisation, involving the orientation of permanent electric dipoles in the direction of the field.

Dielectric polarisation leads to an internal electric field that weakens the external field in the material, thus reducing the effective value of the internal field strength. The magnitude of this effect is described by the relative permeability of the material (εᵣ), which determines the ability of the dielectric to store the energy of the electric field. The greater the permeability, the stronger the polarisation effect.

This phenomenon is of fundamental importance in electrical engineering and electronics, as it affects the operation of Capacitors, waveguides, insulators, as well as the propagation of electromagnetic waves in dielectric media. Under dynamic conditions of an alternating electric field, the response of a material can depend on the frequency, leading to dielectric dispersion phenomena and dielectric losses. In technical applications, the polarisation properties of dielectrics are used in the design of controlled capacitance components, electro-optic materials, sensors and microwave components.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO