+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Potentiometers - definition

A Potentiometer is a three-terminal adjustable resistor whose resistance value can be adjusted by changing the position of a movable contact relative to a resistive element. Its primary function is the precise control of voltage or current in electrical and electronic systems, making it a key component in control, regulation and measurement systems.

Potentiometers' construction includes a stationary resistive path made of materials with stable electrical characteristics, such as carbon, cermet, manganese or conductive polymers, and a movable sliding or rotating slider that modifies the voltage division point. The resistance characteristics can be linear, in which the change in resistance value occurs in proportion to the movement of the slider, or logarithmic, used in audio applications where gain control needs to be adjusted to suit human hearing perception.

Potentiometers' operation is based on the principle of voltage divider, in which the input voltage is divided into two parts according to the current position of the moving contact. In this way, it allows the smooth adjustment of electrical parameters such as volume in acoustic systems, frequency in signal generators or speed in controllers for electric motors.

Depending on the design, potentiometers can be in rotary form, where the adjustment is made by rotating the axis, or in slide form, where the change in resistance is made by moving the contact linearly. For high-precision applications, multi-turn potentiometers are used, allowing a more precise setting of the resistance value. Digital potentiometers use electronic potentiometers where the resistance change is realised by means of switched resistor arrays controlled by binary signals.

Potentiometers' durability and accuracy depend on the quality of the resistive path material and the mechanics of the moving contact, and their wear can lead to a 'shaking' effect resulting from unstable electrical contact. Systems requiring reliability use non-contact potentiometers, such as optical or magnetoresistive encoders, which eliminate the problem of mechanical wear and increase the life of the device.

In industrial automation systems, potentiometers act as angular and linear position sensors, working in conjunction with microprocessor systems and analogue-to-digital converters to enable dynamic control parameters. In audio technology and musical instruments, they are used in audio equalization and signal balancing systems, and in lighting systems they enable stepless regulation of light intensity.

The integration of potentiometers into modern electronic systems includes the use of temperature compensation circuits, miniaturisation in MEMS systems and the implementation of touch technology in control panels, which allows intuitive parameter adjustment in interfaces user interfaces.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO