+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Servo drive - definition

Servo drive is a precision drive system used in Automation and Mechatronics for closed-loop motion control feedback. It consists of a servomotor, a controller (servo amplifier) and a measuring element - usually an encoder or resolver - that allows monitoring of the actual position, speed or torque. The main purpose of the servo drive is to provide dynamic and accurate motion control, adapted to the requirements of the technological process.

Unlike standard Actuators, the servo drive uses feedback to continuously correct the difference between the preset and actual state of motion, thus maintaining high positioning accuracy and stability under varying loads. This makes it suitable for use in machines CNC, robotics, assembly lines, packaging equipment, transport systems and many other applications requiring precise motion control.

Servo drives can operate in positional, velocity or torque modes, and modern systems often integrate these modes within a single system. The servo motors used in servo drives are usually synchronous motors or brushless direct current (BLDC) motors, due to their high efficiency, high power density and ability to be precisely controlled.

The servo controller analyses reference signals (control commands) and compares them with sensor feedback signals, performing real-time control calculations, usually based on PID algorithms or advanced versions thereof. Today's servo drives offer functions for diagnostics, automatic parameter adjustment, network communication (e.g. EtherCAT, CANopen, Modbus) and integration with higher-level control systems.

Thanks to their versatility, responsiveness and high precision, servo drives are a key component of modern systems Automation and robotics, supporting the development of intelligent machines and flexible production lines.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO