+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Electromotive force (SEM) - definition

Electromotive force (SEM, or electromotive force - EMF) is a physical quantity describing the ability of an electrical energy source to induce a flow of charge in a circuit. Although it is expressed in volts (V), like voltage, SEM does not represent the voltage between two points in a purely potential sense, but the total energy supplied by a source per unit charge to overcome the internal and external resistance of a circuit. It is therefore a measure of the work done by the internal mechanism of the source - e.g. a chemical reaction in an electrochemical cell or magnetic induction in a generator - to move an electrical charge.

In the context of Kirchhoff's laws and electrical circuit analysis, the SEM represents the primary energy introduced into the circuit, regardless of losses due to the resistance of the Cables or components. In galvanic cells the electromotive force results from the electrochemical potential difference between electrodes, while in current generators it results from the Lorentz force on charges moving in an alternating magnetic field. SEM also appears in inductive phenomena, e.g. in Coils, where an alternating magnetic field generates a potential difference according to Faraday's law.

From the thermodynamic definition, the electromotive force is the averaged value of the electric field along the closed path taken by the charge in the source. Its value depends on the nature of the source and its operating conditions, such as temperature, chemical composition, magnetic field intensity or frequency of field changes. Despite the name suggesting 'force', it is not a force in the sense of classical mechanics, but a concept corresponding to the difference of potential energy, relevant to the description and design of power systems and electronic devices.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO