+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Contactors is an electromechanical switching apparatus designed to remotely switch on, off and control electrical circuits, especially in high current or high voltage systems. It works on the principle of an electromagnet which, when voltage is applied to the coil, generates a magnetic field that attracts the jumper, causing the set of operating contacts to close or open. When the coils are de-energised, the elastic force causes the contact elements to return to their initial state.
The contactor design distinguishes between essential elements such as the set of main contacts responsible for conducting large operating currents and auxiliary contacts used to perform control and signalling functions in Automation systems. Due to the dynamic nature of their operation, contactors are designed with respect to the resistance to arc arising during switching operations, often through the use of extinguishing chambers.
Contactors are commonly used in industrial applications to control electric motors, pumps, heaters, lighting and in complex automation and process control systems. Their design allows repeated, fast and reliable switching of large loads with minimal wear on the working components. In modern solutions, contactors are found equipped with surge suppression systems , communication interfaces and diagnostic functions, which allows integration with energy management systems and monitoring of equipment operation.
Contactor ratings, such as coil voltage, rated current contacts, switching capacity and category of use (e.g. AC-1, AC-3), must be closely matched to the load characteristics and operating conditions to ensure high mechanical and electrical life of the device.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.