+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Weber (Wb) is a derived unit of the SI system used to measure magnetic flux. It is defined as the amount of magnetic flux that, in a closed electrical circuit causes the induction of an electromotive force of one volt (V), when it undergoes a homogeneous change in one second. Formally, one weber corresponds to one tesla (T) times one square metre (1 Wb = 1 T-m²).
This unit is named after the German physicist Wilhelm Weber, co-founder of electromagnetism, and has been adopted as a standard in electromagnetic nomenclature. Magnetic flux quantitatively describes how strong magnetic field passes through a given surface and is a scalar quantity, being the integral of the magnetic field with respect to the surface through which the field passes.
In practice, the Weber unit is used in the analysis of magnetic circuits, the design of transformers, coils, electric motors, generators and in electromagnetic induction issues. In the context of Faraday's law, the change in magnetic flux over time is the direct cause of electromotive force, which is the fundamental operating principle of many electrical devices.
Since the value of one weber is relatively large compared to typical engineering applications, aliquots of this unit, such as milliweber (mWb) or microweber (μWb), are often used in technical practice. Measuring and analysing magnetic flux using the weber unit enables the precise determination of the magnetic properties of materials and the dynamic characteristics of electromagnetic systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.