+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Solenoid valve a solenoid valve is an electrically operated actuator used in flow systems to control the direction of the, rate and pressure of the working medium, such as gas, liquid or steam. Its operation is based on the conversion of electrical energy into mechanical energy through the phenomenon of electromagnetic induction, which enables fast and precise control of the flow, either remotely or automatically.
The valve design comprises a solenoid made of a coil wound on a core of ferromagnetic and a movable stem, which in its resting position is held by a spring in a closed or open position, depending on the type of valve. When voltage is applied to the coil, a magnetic field is generated magnetic field, which attracts the solenoid, changing the valve state and allowing a controlled fluid flow. Depending on the configuration, solenoid valves can operate in direct action mode, where the solenoids force directly controls the valve position, or in indirect mode, where the pressure of the medium is used to assist opening and closing.
The dynamic properties of solenoid valves depend on coil parameters, such as resistance, inductance and supply voltage, as well as on the mechanical characteristics of the coil system, which determines response time and switching force. High-frequency designs used in precision metering systems use optimised control systems, which reduce the effect of hysteresis magnetic hysteresis and improve the repeatability of switching operations.
Applications for solenoid valves include hydraulic and pneumatic systems, chemical flow control systems, as well as industrial automation equipment, where fast switching and synchronization with digital control systems. In safety installations, they function as shut-off valves, ensuring immediate isolation of the flow in the event of loss of control voltage or detection of emergency parameters of the system operation. Modern production technologies take into account the use of materials resistant to corrosion and aggressive chemical environments, which increases the durability and reliability of valves operating in industrial conditions.
The integration of solenoid valves into control systems includes the implementation of communication interfaces and diagnostic systems enabling real-time monitoring of operating parameters. Automation process systems use models with digital flow control and auto-calibration functions, which allow adaptive adjustment of valve characteristics to changing operating conditions, minimising energy losses and improving the efficiency of the flow control system.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.