+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Profit - definition of

Profit in technical terms, especially in the field of electronics and signal engineering, refers to the ratio of the output signal value to the input signal value in an amplifying or processing system. It is a measure of the ability of a component or system to amplify a signal - it can refer to power, voltage, current or transfer function parameters. Depending on the context, gain can be expressed as an absolute value (the ratio of two quantities) or in decibels (dB), which facilitates the analysis of complex systems, in which signals are subject to successive transformations.

In analog electronics, voltage gain determines, how many times the output signal is greater than the input signal, which is a basic property of operational amplifiers, transistor amplifiers or audio circuits. In radio and communication systems, the term "gain" often refers to the characteristics of Antennas - e.g. antenna gain describes the directivity and efficiency of converting input energy into electromagnetic radiation in a specific direction. In this case, gain also takes into account losses and radiation characteristics, and its value in decibels refers to a dipole antenna or isotropic antenna as a reference point.

In dynamic terms, the gain can depend on frequency, temperature, load impedance and other system operating parameters. In many applications, the key is to ensure stable gain over a wide frequency range, which requires appropriate selection of components and compensation methods. In digital circuits, the concept of gain can be indirectly related to the efficiency of signal processing, although it more often refers to the analog stages of the interfaces.

Gain also plays an important role in control theory and linear systems, where it is part of the system's transmittance function and affects its stability and time response. Regardless of the field, gain analysis makes it possible to assess the quality, efficiency and usability of technical devices and systems in the context of signal processing.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO