+1 500 000 のオファーにある商品数

7000 個の小包が毎日発送されます

150 カ国からの +300 000 の顧客

Quick Buy お気に入り
カート

HONGFA RELAY

Xiamen Hongfa Electroacoustic is a relay manufacturer originating from China. Established in 1984, the company has more than 20 subsidiaries and distributes its products to more than 100 countries and regions. The key product of HONGFA RELAY are relays, which the company produces 1.5 billion units every year. The company also produces contactors, switchgears or installation protections. HONGFA RELAY relays are used, among others in the energy, transport and telecommunications industries. They are also used by manufacturers of medical equipment and household appliances.