+1 500 000 のオファーにある商品数
7000 個の小包が毎日発送されます
150 カ国からの +320 000 の顧客
発行日: 18-08-2023 更新日: 07-11-2026 🕒 8 分钟阅读
Breadboard is a device which makes the construction and prototyping of electronic circuits easier. Many people appreciate the breadboard for its versatility, simplicity and the possibility it gives to build practically any electronic circuit really quickly. Also, breadboards help users learn something new about electronics – that’s because the circuitry can be easily modified as you build it, and in this way numerous novel solutions can be tested.
As the name suggests, ”breadboard” has another meaning, and application, too – it’s a board used to slice up bread. The ambiguity may seem strange, but there’s a good explanation for the double meaning. Before universal methods of prototyping were introduced, electronics engineers constructed circuits on boards that were used to slice up bread. They would attach some circuitry components to the breadboard using nails and screws. The wooden layer guaranteed excellent insulation and made it possible to arrange the components freely across its surface. Therefore, a traditional board used to slice up bread can be perceived as the predecessor of our current breadboards used in electronic circuits.
Breadboards in the TME catalogue
Every electronic circuit consists of a number of components that are connected to each other. In order to check how the circuit works, it has to be designed and built first. There are three ways to construct such a prototype, and each of them has some pros and cons.
Breadboards are made of plastic, with metal tin plates inside, which, once polarised properly, can conduct current. In the outer layer, there are numerous holes placed at a distance of 0.1 inch (2.54 mm) from each other. That’s one of the most common lead pitch, thanks to which most of the electronic components can be used on the breadboard.
Connections in the breadboard
If you want to use breadboards, you should first understand how their components are connected to one another. On the top and bottom edges, there are two rails linked to each other horizontally. Their purpose is to conduct the power to other components. Hence, after we supply power, every hole linked in the same line will receive it. The holes placed in the central part of the breadboard are connected in a different way. They create multiple vertical lines, which are divided in half by a small cavity. This means that there are two columns, and they are marked with digit 1 on the board. One of them is above the cavity, and another one below it.
After understanding the breadboard’s internal structure, it’s time to discuss how to prototype a circuit. It’s a rather simple and quick process, which, undoubtedly, is a crucial advantage of breadboards. The only thing you have to do is place the circuit components on the breadboard, connect the power supply, and the device will be ready for use.
Let’s have a closer look at a simple circuit with an LED, a resistor and a button. The button can be placed above the cavity that is in the central part of the breadboard. In this way, its contacts are available in every hole in column 21 and 23. Now, connect the resistor to the positive powering rail using one pin, and then connect the other one to the column with one button lead. Next, just like in the case of the resistor, connect the LED’s anode to the button, and the cathode to the negative power supply pole. Finally, connect the power supply by plugging the power supply wires into any place on the horizontal rails. Remember, however, not to reverse the poles – on breadboards, the rails are often marked blue for the ground connection and red for the positive power supply pole. It’s worth following the markings, as it may help you avoid problems in the future.
There are many types of breadboards available on the market. They differ from each other mainly in terms of size, which also means that they have various numbers of holes. The most common breadboards have 300 or 820 holes, but there are models with as many as 3000 holes. The choice of the breadboard depends on the desired size of the circuit. Still, it’s worth buying a bit bigger breadboard, as it usually turns out that you could do with a bit more space.
A standard breadboard has two horizontally placed power supply rails, but simpler versions, with only one row of holes, or even without such rails, are available, too.
It's worth noting there’s one more solution to consider – sets of a few breadboards placed on a single base, with additional terminals that make it possible to connect standard wires with banana plugs. It’s quite an interesting product which makes it possible to easily power the circuit using a lab power supply unit.
Every circuit built on a breadboard must be connected properly. With simple circuits, the components’ leads can be connected directly with other leads, but as the circuit expands, it becomes more difficult to do so. A much better solution is to connect the inputs and outputs with the wires dedicated for breadboards. They differ in terms of length and are terminated with a goldpin connector, which fits perfectly into a breadboard opening.
Jumper links could serve as an alternative for standard connection wires. They are more rigid, so they can be used to build neater circuits in which connections are made directly on the breadboard instead of hanging loosely. Many hobbyists build their own jumper links from Ethernet cables, but it’s not the best solution. Such wires are made of copper, which is fragile, and their terminals aren’t tinned.
Beside the previously mentioned connection wires, there are many other accessories for breadboards. Above all, these include power supply modules which are plugged directly to the breadboard in order to supply power from a standard PSU using a DC plug. What’s more, quite a lot of adapters dedicated for breadboards are available. They can be used to connect, for example, a USB cable, FFC ribbon cable or even a HDMI connector to a breadboard. In fact, our imagination is the only limitation – if you want to connect something to a breadboard, it’s highly likely that an appropriate adapter already exists. However, if it’s not there, it may be a perfect opportunity to invent one on your own.
Transfer Multisort Elektronik(TME)は、電子部品、電気・電子機器、作業工具、ならびに産業用オートメーション機器を取り扱う世界有数のグローバルディストリビューターです。TMEのカタログには、1300社以上の主要メーカーによる150万点を超える製品が掲載されています。ウッチ市およびルズグフ市に所在するTMEの最新物流センターは、総面積40,000㎡以上を有し、毎日約6,000個の電子部品関連パッケージを、150か国以上の顧客へ発送しています。
TME はまた、TME Education プロジェクトを通じて若手エンジニアや電子工学愛好家の知識とスキルの向上に取り組み、TechMasterEvent シリーズを開催して技術コミュニティを支援し、イノベーションと経験の共有を促進しています。