+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

접촉기

(7 469)

Contactor – what is a contactor and what is it used for?

A contactor is a type of electric switch. Its design and method of operation are similar to those of an electromagnetic relay. Unlike relays, contactors are used for switching main circuits, while relays – for switching auxiliary circuits. Contactors tolerate electrical surges and overvoltage well. They are characterized by high mechanical durability and allow to achieve a high switching frequency at very high operational reliability.

Contactor – differences between contactors and relays

Contactors differ from the relays not only in terms of their intended use, but also in their construction, as in general they are designed to conduct very high currents. In simple terms, it can be said that although their principle of operation is the same (transmitting an electrical signal after contacts are short-circuited) as that of electromagnetic relays, you can easily distinguish a contactor from a relay at first glance, because usually contactors have a large casing and a distinctive shape.

Contactors are capable of switching highly inductive or capacitive loads. They can be used, for example, to start a powerful electric motor. Relays are used to transmit control signals, including those that switch on the contactor. Relay contacts have a rather small current load capacity (typically up to 10 A) and coil voltage within the range of 5 to 24V. Moreover, a relay has a significantly smaller electromagnet than a contactor, and its contacts do not have any additional devices for electric arc extinguishing.

What is important, the contactor’s contact switching time is longer than in the case of a relay. Contactors (except for the quiet ones) work much louder than the relays.

Contactors – control and power supply methods

A contactor is switched on and powered in the same way as an electromagnetic relay. Its electromagnet is powered with a higher voltage than in the case of a relay. The coil rated voltage in certain versions of a contactor can reach up to 500V DC. Typically used values are: 12V DC/AC, 24V DC/AC, 48V DC, 110V AC, 230V AC.

Contactors – basic parameters

The basic parameters of a contactor include: contact configuration, maximum load current, coil control voltage and insulation voltage. In some applications, additional accessories, such as auxiliary contacts enabling to signal the operation of the contactor or to switch on the auxiliary circuit, will also be very important.

Choosing a right contactor for your application

The choice of a contactor depends on its function, the value of the switched current and voltage, type of voltage (AC/DC) and type of load. In order to choose a right contactor, one should know the circuit parameters mentioned before and choose a contactor with a rated current that is not lower than the one stated there. If used intensively in industrial applications, a contactor with the operating capability of the current specifications should be chosen, in which contacts can handle twice (or more) the load. It prolongs the service life of frequently switched contactors.

A contactor will prove useful in switching electric motors, heaters, pumps, sirens, fluorescent lamps, fans and other high-power electrical equipment

Accessories for contactors

Manufacturers offer many accessories for contactors, for example: auxiliary contacts, mechanical lock-out latches to maintain the contactor status, electronic timer modules to switch the contactor off or on after a certain time and overvoltage protectors.

제품: 7 469

창고:

TME
외부의
전부
페이지 1
LADN22 | 보조 접점; 나사 단자; 정면; 접점: NC x2 + NO x2; TeSys D
보조 접점; 나사 단자; 정면; 접점: NC x2 + NO x2; TeSys D
제조업체 부품 번호: LADN22
다음의 수량에 대한 순 가격 1 pcs - 15.82 USD다음의 수량에 대한 총 가격 1 pcs - 15.82 USD
다음의 수량에 대한 순 가격 10 pcs - 14.84 USD다음의 수량에 대한 총 가격 10 pcs - 14.84 USD
다음의 수량에 대한 순 가격 20 pcs - 13.85 USD다음의 수량에 대한 총 가격 20 pcs - 13.85 USD
555 TME에 재고 있음
개 번호 (다양성: 1)
3RH2911-1FA22 | 보조 접점; 크기: S0,S00,S2; 나사 단자; 정면; 접점: NC x2 + NO x2; 3RT20
보조 접점; 크기: S0,S00,S2; 나사 단자; 정면; 접점: NC x2 + NO x2; 3RT20
제조업체 부품 번호: 3RH2911-1FA22
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 11.74 USD다음의 수량에 대한 총 가격 1 pcs - 11.74 USD
다음의 수량에 대한 순 가격 5 pcs - 11.10 USD다음의 수량에 대한 총 가격 5 pcs - 11.10 USD
다음의 수량에 대한 순 가격 10 pcs - 10.38 USD다음의 수량에 대한 총 가격 10 pcs - 10.38 USD
196 TME에 재고 있음
개 번호 (다양성: 1)
3RT2016-1BB41 | 접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 9A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 9A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
제조업체 부품 번호: 3RT2016-1BB41
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 30.90 USD다음의 수량에 대한 총 가격 1 pcs - 30.90 USD
다음의 수량에 대한 순 가격 5 pcs - 29.22 USD다음의 수량에 대한 총 가격 5 pcs - 29.22 USD
다음의 수량에 대한 순 가격 10 pcs - 27.16 USD다음의 수량에 대한 총 가격 10 pcs - 27.16 USD
322 TME에 재고 있음
개 번호 (다양성: 1)
LADN11 | 보조 접점; 나사 단자; 정면; 접점: NC + NO; TeSys D
보조 접점; 나사 단자; 정면; 접점: NC + NO; TeSys D
제조업체 부품 번호: LADN11
다음의 수량에 대한 순 가격 1 pcs - 8.86 USD다음의 수량에 대한 총 가격 1 pcs - 8.86 USD
다음의 수량에 대한 순 가격 10 pcs - 8.30 USD다음의 수량에 대한 총 가격 10 pcs - 8.30 USD
다음의 수량에 대한 순 가격 20 pcs - 7.75 USD다음의 수량에 대한 총 가격 20 pcs - 7.75 USD
468 TME에 재고 있음
개 번호 (다양성: 1)
3RT2016-1BB42 | 접촉기: 3극; NO x3; 보조 접점: NC; 24VDC; 9A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NC; 24VDC; 9A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
제조업체 부품 번호: 3RT2016-1BB42
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 30.90 USD다음의 수량에 대한 총 가격 1 pcs - 30.90 USD
다음의 수량에 대한 순 가격 5 pcs - 29.22 USD다음의 수량에 대한 총 가격 5 pcs - 29.22 USD
다음의 수량에 대한 순 가격 10 pcs - 27.16 USD다음의 수량에 대한 총 가격 10 pcs - 27.16 USD
293 TME에 재고 있음
개 번호 (다양성: 1)
3RT2026-1BB40 | 접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 25A; 패널에,DIN 레일 장착용; 3RT20
접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 25A; 패널에,DIN 레일 장착용; 3RT20
제조업체 부품 번호: 3RT2026-1BB40
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 96.89 USD다음의 수량에 대한 총 가격 1 pcs - 96.89 USD
다음의 수량에 대한 순 가격 5 pcs - 91.60 USD다음의 수량에 대한 총 가격 5 pcs - 91.60 USD
다음의 수량에 대한 순 가격 10 pcs - 85.15 USD다음의 수량에 대한 총 가격 10 pcs - 85.15 USD
142 TME에 재고 있음
개 번호 (다양성: 1)
GMD-16M 24VDC 1A | 접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 16A; 패널에,DIN 레일 장착용; METAMEC; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 16A; 패널에,DIN 레일 장착용; METAMEC; 나사 단자
제조업체 부품 번호: GMD-16M 24VDC 1A
제조사: LS ELECTRIC
다음의 수량에 대한 순 가격 1 pcs - 21.05 USD다음의 수량에 대한 총 가격 1 pcs - 21.05 USD
다음의 수량에 대한 순 가격 5 pcs - 19.81 USD다음의 수량에 대한 총 가격 5 pcs - 19.81 USD
다음의 수량에 대한 순 가격 10 pcs - 18.57 USD다음의 수량에 대한 총 가격 10 pcs - 18.57 USD
다음의 수량에 대한 순 가격 25 pcs - 17.34 USD다음의 수량에 대한 총 가격 25 pcs - 17.34 USD
285 TME에 재고 있음
개 번호 (다양성: 1)
LC1D09BL | 접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 9A; 패널에,DIN 레일 장착용; TeSys D
접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 9A; 패널에,DIN 레일 장착용; TeSys D
제조업체 부품 번호: LC1D09BL
다음의 수량에 대한 순 가격 1 pcs - 41.20 USD다음의 수량에 대한 총 가격 1 pcs - 41.20 USD
다음의 수량에 대한 순 가격 5 pcs - 38.63 USD다음의 수량에 대한 총 가격 5 pcs - 38.63 USD
다음의 수량에 대한 순 가격 10 pcs - 36.05 USD다음의 수량에 대한 총 가격 10 pcs - 36.05 USD
200 TME에 재고 있음
개 번호 (다양성: 1)
3RT2916-1DG00 | 서지 피뢰기; 잡음 억제 다이오드; 크기: S00; 12÷250VDC; 3RT20
서지 피뢰기; 잡음 억제 다이오드; 크기: S00; 12÷250VDC; 3RT20
제조업체 부품 번호: 3RT2916-1DG00
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 7.04 USD다음의 수량에 대한 총 가격 1 pcs - 7.04 USD
다음의 수량에 대한 순 가격 5 pcs - 6.65 USD다음의 수량에 대한 총 가격 5 pcs - 6.65 USD
다음의 수량에 대한 순 가격 10 pcs - 6.19 USD다음의 수량에 대한 총 가격 10 pcs - 6.19 USD
445 TME에 재고 있음
개 번호 (다양성: 1)
LA1KN22 | 보조 접점; 나사 단자; 정면; 접점: NC x2 + NO x2; TeSys K
보조 접점; 나사 단자; 정면; 접점: NC x2 + NO x2; TeSys K
제조업체 부품 번호: LA1KN22
다음의 수량에 대한 순 가격 1 pcs - 13.17 USD다음의 수량에 대한 총 가격 1 pcs - 13.17 USD
다음의 수량에 대한 순 가격 3 pcs - 12.49 USD다음의 수량에 대한 총 가격 3 pcs - 12.49 USD
323 TME에 재고 있음
개 번호 (다양성: 1)
3RT2015-1BB42 | 접촉기: 3극; NO x3; 보조 접점: NC; 24VDC; 7A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NC; 24VDC; 7A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
제조업체 부품 번호: 3RT2015-1BB42
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 28.96 USD다음의 수량에 대한 총 가격 1 pcs - 28.96 USD
다음의 수량에 대한 순 가격 5 pcs - 27.39 USD다음의 수량에 대한 총 가격 5 pcs - 27.39 USD
다음의 수량에 대한 순 가격 10 pcs - 25.45 USD다음의 수량에 대한 총 가격 10 pcs - 25.45 USD
269 TME에 재고 있음
개 번호 (다양성: 1)
LC1D09P7 | 접촉기: 3극; NO x3; 보조 접점: NO + NC; 230VAC; 9A; 패널에,DIN 레일 장착용; TeSys D
접촉기: 3극; NO x3; 보조 접점: NO + NC; 230VAC; 9A; 패널에,DIN 레일 장착용; TeSys D
제조업체 부품 번호: LC1D09P7
다음의 수량에 대한 순 가격 1 pcs - 30.73 USD다음의 수량에 대한 총 가격 1 pcs - 30.73 USD
다음의 수량에 대한 순 가격 5 pcs - 28.49 USD다음의 수량에 대한 총 가격 5 pcs - 28.49 USD
다음의 수량에 대한 순 가격 10 pcs - 26.46 USD다음의 수량에 대한 총 가격 10 pcs - 26.46 USD
262 TME에 재고 있음
개 번호 (다양성: 1)
LP1K1201BD | 접촉기: 3극; NO x3; 보조 접점: NC; 24VDC; 12A; 패널에,DIN 레일 장착용; TeSys K; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NC; 24VDC; 12A; 패널에,DIN 레일 장착용; TeSys K; 나사 단자
제조업체 부품 번호: LP1K1201BD
다음의 수량에 대한 순 가격 1 pcs - 37.39 USD다음의 수량에 대한 총 가격 1 pcs - 37.39 USD
다음의 수량에 대한 순 가격 5 pcs - 35.29 USD다음의 수량에 대한 총 가격 5 pcs - 35.29 USD
다음의 수량에 대한 순 가격 10 pcs - 32.72 USD다음의 수량에 대한 총 가격 10 pcs - 32.72 USD
321 TME에 재고 있음
개 번호 (다양성: 1)
22.32.0.024.4320 | 접촉기: 2극 장치; 25A; 24VAC,24VDC; NO x2; DIN 레일 장착용; IP20; 22; -25÷50°C
접촉기: 2극 장치; 25A; 24VAC,24VDC; NO x2; DIN 레일 장착용; IP20; 22; -25÷50°C
제조업체 부품 번호: 22.32.0.024.4320
제조사: FINDER
다음의 수량에 대한 순 가격 1 pcs - 37.41 USD다음의 수량에 대한 총 가격 1 pcs - 37.41 USD
다음의 수량에 대한 순 가격 5 pcs - 35.23 USD다음의 수량에 대한 총 가격 5 pcs - 35.23 USD
다음의 수량에 대한 순 가격 10 pcs - 34.14 USD다음의 수량에 대한 총 가격 10 pcs - 34.14 USD
273 TME에 재고 있음
개 번호 (다양성: 1)
LC1D09BD | 접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 9A; 패널에,DIN 레일 장착용; TeSys D
접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 9A; 패널에,DIN 레일 장착용; TeSys D
제조업체 부품 번호: LC1D09BD
다음의 수량에 대한 순 가격 1 pcs - 59.54 USD다음의 수량에 대한 총 가격 1 pcs - 59.54 USD
다음의 수량에 대한 순 가격 5 pcs - 55.57 USD다음의 수량에 대한 총 가격 5 pcs - 55.57 USD
다음의 수량에 대한 순 가격 10 pcs - 51.60 USD다음의 수량에 대한 총 가격 10 pcs - 51.60 USD
282 TME에 재고 있음
개 번호 (다양성: 1)
1SBL137001R1110 | 접촉기: 3극; NO x3; 보조 접점: NO; 24÷60VAC,20÷60VDC; 9A; 패널에,DIN 레일 장착용; AF
접촉기: 3극; NO x3; 보조 접점: NO; 24÷60VAC,20÷60VDC; 9A; 패널에,DIN 레일 장착용; AF
제조업체 부품 번호: 1SBL137001R1110
제조사: ABB
다음의 수량에 대한 순 가격 1 pcs - 36.16 USD다음의 수량에 대한 총 가격 1 pcs - 36.16 USD
다음의 수량에 대한 순 가격 5 pcs - 34.09 USD다음의 수량에 대한 총 가격 5 pcs - 34.09 USD
다음의 수량에 대한 순 가격 10 pcs - 32.02 USD다음의 수량에 대한 총 가격 10 pcs - 32.02 USD
156 TME에 재고 있음
개 번호 (다양성: 1)
LC1D25P7 | 접촉기: 3극; NO x3; 보조 접점: NO + NC; 230VAC; 25A; 패널에,DIN 레일 장착용; TeSys D
접촉기: 3극; NO x3; 보조 접점: NO + NC; 230VAC; 25A; 패널에,DIN 레일 장착용; TeSys D
제조업체 부품 번호: LC1D25P7
다음의 수량에 대한 순 가격 1 pcs - 63.68 USD다음의 수량에 대한 총 가격 1 pcs - 63.68 USD
다음의 수량에 대한 순 가격 5 pcs - 59.43 USD다음의 수량에 대한 총 가격 5 pcs - 59.43 USD
다음의 수량에 대한 순 가격 10 pcs - 55.19 USD다음의 수량에 대한 총 가격 10 pcs - 55.19 USD
251 TME에 재고 있음
개 번호 (다양성: 1)
LC1D18BD | 접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 18A; 패널에,DIN 레일 장착용; TeSys D
접촉기: 3극; NO x3; 보조 접점: NO + NC; 24VDC; 18A; 패널에,DIN 레일 장착용; TeSys D
제조업체 부품 번호: LC1D18BD
다음의 수량에 대한 순 가격 1 pcs - 79.31 USD다음의 수량에 대한 총 가격 1 pcs - 79.31 USD
다음의 수량에 대한 순 가격 5 pcs - 74.02 USD다음의 수량에 대한 총 가격 5 pcs - 74.02 USD
다음의 수량에 대한 순 가격 10 pcs - 68.74 USD다음의 수량에 대한 총 가격 10 pcs - 68.74 USD
188 TME에 재고 있음
개 번호 (다양성: 1)
3RT2015-1BB41 | 접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 7A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 7A; 패널에,DIN 레일 장착용; 3RT20; 나사 단자
제조업체 부품 번호: 3RT2015-1BB41
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 28.96 USD다음의 수량에 대한 총 가격 1 pcs - 28.96 USD
다음의 수량에 대한 순 가격 5 pcs - 27.39 USD다음의 수량에 대한 총 가격 5 pcs - 27.39 USD
다음의 수량에 대한 순 가격 10 pcs - 25.45 USD다음의 수량에 대한 총 가격 10 pcs - 25.45 USD
96 TME에 재고 있음
개 번호 (다양성: 1)
LP1K0910BD | 접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 9A; 패널에,DIN 레일 장착용; TeSys K; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 9A; 패널에,DIN 레일 장착용; TeSys K; 나사 단자
제조업체 부품 번호: LP1K0910BD
다음의 수량에 대한 순 가격 1 pcs - 32.27 USD다음의 수량에 대한 총 가격 1 pcs - 32.27 USD
다음의 수량에 대한 순 가격 5 pcs - 30.06 USD다음의 수량에 대한 총 가격 5 pcs - 30.06 USD
다음의 수량에 대한 순 가격 10 pcs - 28.26 USD다음의 수량에 대한 총 가격 10 pcs - 28.26 USD
180 TME에 재고 있음
개 번호 (다양성: 1)
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용