+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

코일 와이어

(411)

Coil wires – a universal selection for the majority of electrical installations

Coil wires are a special group of wires in electrical installations. They are successfully used in automotive industry or ICT as a part of power supply systems. However, their primary application is the production of transformers, inductors, and electromagnets. A catalogue of coil wires available at TME contains different types of wires adapted to electrical installations operating in various conditions.

Coil wire – quality. What to pay attention to?

Good electrical conductivity is ensured by wires made of pure metals, especially copper. A coil wire has its core made of high-quality copper annealed and electrolytically refined during production, which differentiates it from other wires. This is especially important in the production of inductors, as their inductance depends on the number and thickness of turns. With coil wires, more turns can be wound, which makes the inductor more useful without changing its dimensions. Apart from that, high-quality anaerobic copper is also used to manufacture coil wires used in hydrogen-cooled generators or motors. The main distinguishing feature of a coil wire is the thin insulation layer made of enamel applied onto the copper core. TME offers copper coil wires from SYNFLEX, coated with two different insulation layers, which allows them to be used in particularly harsh conditions. They work excellent in propulsion systems, transformers, or power tools exposed to high temperatures or corrosive substances.

Coil wires – selection based on available parameters

Coil wires available at TME are selected based on many different factors, such as wire thickness and shape, operating temperature range, or insulation class.

Coil wires with small diameter usually have a round cross-section. They are primarily used in manufacturing transducers or in applications requiring compact size of components. Coil wires with larger diameters have cross-sections in the shape of a square or even a hexagon, which allows for a more efficient transport. Also, such shapes ensure better thermal conductivity between subsequent turns. TME Catalogue comprises coil wires with a wide range of diameters from renowned manufacturers, as well as bespoke products prepared on request.

Coil wires have the so-called operating temperature range. This is the temperature of the wire after 20,000 hours of usage. The lower the temperature, the longer the operating time (ca. twice for every 10°C).

The insulation of the wire with copper core protects it against harmful environmental conditions. On top of that, it also works as a protection against electro-static discharges caused by free electrons in the insulator. There are three types of insulation, which differ in terms of thickness. It should be mentioned that in order to connect two coil wires together or attach a wire to an existing installation, the insulation has to be removed. Getting rid of the enamel is usually troublesome. That’s why on request, we can adapt coil wires to our customers’ needs. Prices are negotiable in case of large orders.

Wide selection of coil wires at TME

Due to the use of coil wires, the inductance of electrical coils was improved while saving the material and improving their overall quality. In propulsion systems using these wires, lower energy losses were observed. In the past, energy losses were caused by coil resistance. Apart from that, the abovementioned propulsion systems now generate considerably less heat during the conversion of electrical energy to kinetic energy.

Our offer comprises a wide selection of coil wires characterised by high quality of materials, wide temperature ranges, and a broad selection of wire diameters.

제품: 411

창고:

TME
전부
페이지 1
DN2E0,20-200G | 코일 와이어; 이중 코팅 에나멜; 0.2mm; 0.2kg; -65÷180°C; 핵심: Cu; 포장: 602m
코일 와이어; 이중 코팅 에나멜; 0.2mm; 0.2kg; -65÷180°C; 핵심: Cu; 포장: 602m
제조업체 부품 번호: DN2E0,20-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 16.11 USD다음의 수량에 대한 총 가격 1 rol - 16.11 USD
다음의 수량에 대한 순 가격 3 rol - 13.92 USD다음의 수량에 대한 총 가격 3 rol - 13.92 USD
다음의 수량에 대한 순 가격 5 rol - 12.45 USD다음의 수량에 대한 총 가격 5 rol - 12.45 USD
다음의 수량에 대한 순 가격 10 rol - 10.99 USD다음의 수량에 대한 총 가격 10 rol - 10.99 USD
23 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E0,30-200G | 코일 와이어; 이중 코팅 에나멜; 0.3mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 302m
코일 와이어; 이중 코팅 에나멜; 0.3mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 302m
제조업체 부품 번호: DN2E0,30-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 15.52 USD다음의 수량에 대한 총 가격 1 rol - 15.52 USD
다음의 수량에 대한 순 가격 3 rol - 13.40 USD다음의 수량에 대한 총 가격 3 rol - 13.40 USD
다음의 수량에 대한 순 가격 5 rol - 11.99 USD다음의 수량에 대한 총 가격 5 rol - 11.99 USD
다음의 수량에 대한 순 가격 10 rol - 10.58 USD다음의 수량에 대한 총 가격 10 rol - 10.58 USD
0 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
1040 0300 44 | 코일 와이어; 단일 코팅 에나멜; 0.3mm; 0.25kg; max.180°C; 핵심: Cu; 포장: 395m; V 180
코일 와이어; 단일 코팅 에나멜; 0.3mm; 0.25kg; max.180°C; 핵심: Cu; 포장: 395m; V 180
제조업체 부품 번호: 1040 0300 44
제조사: SYNFLEX
다음의 수량에 대한 순 가격 1 rol - 15.63 USD다음의 수량에 대한 총 가격 1 rol - 15.63 USD
다음의 수량에 대한 순 가격 3 rol - 13.68 USD다음의 수량에 대한 총 가격 3 rol - 13.68 USD
다음의 수량에 대한 순 가격 5 rol - 12.70 USD다음의 수량에 대한 총 가격 5 rol - 12.70 USD
19 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E0,40-200G | 코일 와이어; 이중 코팅 에나멜; 0.4mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 171m
코일 와이어; 이중 코팅 에나멜; 0.4mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 171m
제조업체 부품 번호: DN2E0,40-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 11.94 USD다음의 수량에 대한 총 가격 1 rol - 11.94 USD
다음의 수량에 대한 순 가격 3 rol - 10.31 USD다음의 수량에 대한 총 가격 3 rol - 10.31 USD
다음의 수량에 대한 순 가격 5 rol - 9.22 USD다음의 수량에 대한 총 가격 5 rol - 9.22 USD
다음의 수량에 대한 순 가격 10 rol - 8.14 USD다음의 수량에 대한 총 가격 10 rol - 8.14 USD
11 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E0,15-200G | 코일 와이어; 이중 코팅 에나멜; 0.15mm; 0.2kg; -65÷180°C; 핵심: Cu; 포장: 1197m
코일 와이어; 이중 코팅 에나멜; 0.15mm; 0.2kg; -65÷180°C; 핵심: Cu; 포장: 1197m
제조업체 부품 번호: DN2E0,15-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 17.91 USD다음의 수량에 대한 총 가격 1 rol - 17.91 USD
다음의 수량에 대한 순 가격 3 rol - 15.46 USD다음의 수량에 대한 총 가격 3 rol - 15.46 USD
다음의 수량에 대한 순 가격 5 rol - 13.84 USD다음의 수량에 대한 총 가격 5 rol - 13.84 USD
다음의 수량에 대한 순 가격 10 rol - 12.21 USD다음의 수량에 대한 총 가격 10 rol - 12.21 USD
2 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E0,50-200G | 코일 와이어; 이중 코팅 에나멜; 0.5mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 110m
코일 와이어; 이중 코팅 에나멜; 0.5mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 110m
제조업체 부품 번호: DN2E0,50-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 11.94 USD다음의 수량에 대한 총 가격 1 rol - 11.94 USD
다음의 수량에 대한 순 가격 3 rol - 10.31 USD다음의 수량에 대한 총 가격 3 rol - 10.31 USD
다음의 수량에 대한 순 가격 5 rol - 9.22 USD다음의 수량에 대한 총 가격 5 rol - 9.22 USD
다음의 수량에 대한 순 가격 10 rol - 8.14 USD다음의 수량에 대한 총 가격 10 rol - 8.14 USD
14 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
1040 0500 44 | 코일 와이어; 단일 코팅 에나멜; 0.5mm; 0.25kg; max.180°C; 핵심: Cu; 포장: 142m; V 180
코일 와이어; 단일 코팅 에나멜; 0.5mm; 0.25kg; max.180°C; 핵심: Cu; 포장: 142m; V 180
제조업체 부품 번호: 1040 0500 44
제조사: SYNFLEX
다음의 수량에 대한 순 가격 1 rol - 13.91 USD다음의 수량에 대한 총 가격 1 rol - 13.91 USD
다음의 수량에 대한 순 가격 3 rol - 12.17 USD다음의 수량에 대한 총 가격 3 rol - 12.17 USD
다음의 수량에 대한 순 가격 5 rol - 11.30 USD다음의 수량에 대한 총 가격 5 rol - 11.30 USD
0 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E1,00-200G | 코일 와이어; 이중 코팅 에나멜; 1mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 28m
코일 와이어; 이중 코팅 에나멜; 1mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 28m
제조업체 부품 번호: DN2E1,00-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 11.19 USD다음의 수량에 대한 총 가격 1 rol - 11.19 USD
다음의 수량에 대한 순 가격 3 rol - 9.67 USD다음의 수량에 대한 총 가격 3 rol - 9.67 USD
다음의 수량에 대한 순 가격 5 rol - 8.65 USD다음의 수량에 대한 총 가격 5 rol - 8.65 USD
다음의 수량에 대한 순 가격 10 rol - 7.63 USD다음의 수량에 대한 총 가격 10 rol - 7.63 USD
9 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DNE0,06-200G | 코일 와이어; 단일 코팅 에나멜; 0.06mm; 0.2kg; -65÷155°C; 핵심: Cu; 포장: 7558m
코일 와이어; 단일 코팅 에나멜; 0.06mm; 0.2kg; -65÷155°C; 핵심: Cu; 포장: 7558m
제조업체 부품 번호: DNE0,06-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 42.71 USD다음의 수량에 대한 총 가격 1 rol - 42.71 USD
다음의 수량에 대한 순 가격 3 rol - 36.72 USD다음의 수량에 대한 총 가격 3 rol - 36.72 USD
다음의 수량에 대한 순 가격 5 rol - 32.85 USD다음의 수량에 대한 총 가격 5 rol - 32.85 USD
다음의 수량에 대한 순 가격 10 rol - 28.99 USD다음의 수량에 대한 총 가격 10 rol - 28.99 USD
9 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
1030 1000 44 | 코일 와이어; 단일 코팅 에나멜; 1mm; 0.25kg; max.200°C; 핵심: Cu; 포장: 36m; W 210
코일 와이어; 단일 코팅 에나멜; 1mm; 0.25kg; max.200°C; 핵심: Cu; 포장: 36m; W 210
제조업체 부품 번호: 1030 1000 44
제조사: SYNFLEX
다음의 수량에 대한 순 가격 1 rol - 12.71 USD다음의 수량에 대한 총 가격 1 rol - 12.71 USD
다음의 수량에 대한 순 가격 3 rol - 11.12 USD다음의 수량에 대한 총 가격 3 rol - 11.12 USD
다음의 수량에 대한 순 가격 5 rol - 10.33 USD다음의 수량에 대한 총 가격 5 rol - 10.33 USD
11 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DNE0,20-200G | 코일 와이어; 단일 코팅 에나멜; 0.2mm; 0.2kg; -65÷155°C; 핵심: Cu; 포장: 680m
코일 와이어; 단일 코팅 에나멜; 0.2mm; 0.2kg; -65÷155°C; 핵심: Cu; 포장: 680m
제조업체 부품 번호: DNE0,20-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 16.11 USD다음의 수량에 대한 총 가격 1 rol - 16.11 USD
다음의 수량에 대한 순 가격 3 rol - 13.92 USD다음의 수량에 대한 총 가격 3 rol - 13.92 USD
다음의 수량에 대한 순 가격 5 rol - 12.45 USD다음의 수량에 대한 총 가격 5 rol - 12.45 USD
다음의 수량에 대한 순 가격 10 rol - 10.99 USD다음의 수량에 대한 총 가격 10 rol - 10.99 USD
8 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DNE0,10-200G | 코일 와이어; 단일 코팅 에나멜; 0.1mm; 0.2kg; -65÷155°C; 핵심: Cu; 포장: 2744m
코일 와이어; 단일 코팅 에나멜; 0.1mm; 0.2kg; -65÷155°C; 핵심: Cu; 포장: 2744m
제조업체 부품 번호: DNE0,10-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 39.08 USD다음의 수량에 대한 총 가격 1 rol - 39.08 USD
다음의 수량에 대한 순 가격 3 rol - 33.75 USD다음의 수량에 대한 총 가격 3 rol - 33.75 USD
다음의 수량에 대한 순 가격 5 rol - 30.20 USD다음의 수량에 대한 총 가격 5 rol - 30.20 USD
다음의 수량에 대한 순 가격 10 rol - 26.65 USD다음의 수량에 대한 총 가격 10 rol - 26.65 USD
8 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E0,60-200G | 코일 와이어; 이중 코팅 에나멜; 0.6mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 78m
코일 와이어; 이중 코팅 에나멜; 0.6mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 78m
제조업체 부품 번호: DN2E0,60-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 12.08 USD다음의 수량에 대한 총 가격 1 rol - 12.08 USD
다음의 수량에 대한 순 가격 3 rol - 10.44 USD다음의 수량에 대한 총 가격 3 rol - 10.44 USD
다음의 수량에 대한 순 가격 5 rol - 9.34 USD다음의 수량에 대한 총 가격 5 rol - 9.34 USD
다음의 수량에 대한 순 가격 10 rol - 8.24 USD다음의 수량에 대한 총 가격 10 rol - 8.24 USD
5 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
1040 0400 44 | 코일 와이어; 단일 코팅 에나멜; 0.4mm; 0.25kg; max.180°C; 핵심: Cu; 포장: 199m; V 180
코일 와이어; 단일 코팅 에나멜; 0.4mm; 0.25kg; max.180°C; 핵심: Cu; 포장: 199m; V 180
제조업체 부품 번호: 1040 0400 44
제조사: SYNFLEX
다음의 수량에 대한 순 가격 1 rol - 14.69 USD다음의 수량에 대한 총 가격 1 rol - 14.69 USD
다음의 수량에 대한 순 가격 3 rol - 12.86 USD다음의 수량에 대한 총 가격 3 rol - 12.86 USD
다음의 수량에 대한 순 가격 5 rol - 11.94 USD다음의 수량에 대한 총 가격 5 rol - 11.94 USD
0 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
1030 1000 47 | 코일 와이어; 단일 코팅 에나멜; 1mm; 1kg; max.200°C; 핵심: Cu; 포장: 142m; W 210
코일 와이어; 단일 코팅 에나멜; 1mm; 1kg; max.200°C; 핵심: Cu; 포장: 142m; W 210
제조업체 부품 번호: 1030 1000 47
제조사: SYNFLEX
다음의 수량에 대한 순 가격 1 rol - 42.01 USD다음의 수량에 대한 총 가격 1 rol - 42.01 USD
다음의 수량에 대한 순 가격 3 rol - 36.54 USD다음의 수량에 대한 총 가격 3 rol - 36.54 USD
다음의 수량에 대한 순 가격 5 rol - 33.93 USD다음의 수량에 대한 총 가격 5 rol - 33.93 USD
0 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
1030 0800 44 | 코일 와이어; 단일 코팅 에나멜; 0.8mm; 0.25kg; max.200°C; 핵심: Cu; 포장: 56m; W 210
코일 와이어; 단일 코팅 에나멜; 0.8mm; 0.25kg; max.200°C; 핵심: Cu; 포장: 56m; W 210
제조업체 부품 번호: 1030 0800 44
제조사: SYNFLEX
다음의 수량에 대한 순 가격 1 rol - 12.86 USD다음의 수량에 대한 총 가격 1 rol - 12.86 USD
다음의 수량에 대한 순 가격 3 rol - 11.25 USD다음의 수량에 대한 총 가격 3 rol - 11.25 USD
다음의 수량에 대한 순 가격 5 rol - 10.45 USD다음의 수량에 대한 총 가격 5 rol - 10.45 USD
15 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E0,80-200G | 코일 와이어; 이중 코팅 에나멜; 0.8mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 44m
코일 와이어; 이중 코팅 에나멜; 0.8mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 44m
제조업체 부품 번호: DN2E0,80-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 11.64 USD다음의 수량에 대한 총 가격 1 rol - 11.64 USD
다음의 수량에 대한 순 가격 3 rol - 10.05 USD다음의 수량에 대한 총 가격 3 rol - 10.05 USD
다음의 수량에 대한 순 가격 5 rol - 8.99 USD다음의 수량에 대한 총 가격 5 rol - 8.99 USD
다음의 수량에 대한 순 가격 10 rol - 7.94 USD다음의 수량에 대한 총 가격 10 rol - 7.94 USD
8 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E0.15/0.25 | 코일 와이어; 이중 코팅 에나멜; 0.15mm; 0.25kg; -65÷200°C; 핵심: Cu; 포장: 1.6km
코일 와이어; 이중 코팅 에나멜; 0.15mm; 0.25kg; -65÷200°C; 핵심: Cu; 포장: 1.6km
제조업체 부품 번호: DN2E0.15/0.25
제조사: BQ CABLE
다음의 수량에 대한 순 가격 1 rol - 41.88 USD다음의 수량에 대한 총 가격 1 rol - 41.88 USD
다음의 수량에 대한 순 가격 3 rol - 36.30 USD다음의 수량에 대한 총 가격 3 rol - 36.30 USD
10 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DN2E1,20-200G | 코일 와이어; 이중 코팅 에나멜; 1.2mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 19m
코일 와이어; 이중 코팅 에나멜; 1.2mm; 0.2kg; -65÷200°C; 핵심: Cu; 포장: 19m
제조업체 부품 번호: DN2E1,20-200G
제조사: INDEL
다음의 수량에 대한 순 가격 1 rol - 11.34 USD다음의 수량에 대한 총 가격 1 rol - 11.34 USD
다음의 수량에 대한 순 가격 3 rol - 9.79 USD다음의 수량에 대한 총 가격 3 rol - 9.79 USD
다음의 수량에 대한 순 가격 5 rol - 8.76 USD다음의 수량에 대한 총 가격 5 rol - 8.76 USD
다음의 수량에 대한 순 가격 10 rol - 7.73 USD다음의 수량에 대한 총 가격 10 rol - 7.73 USD
5 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
1030 1500 44 | 코일 와이어; 단일 코팅 에나멜; 1.5mm; 0.25kg; max.200°C; 핵심: Cu; 포장: 16m; W 210
코일 와이어; 단일 코팅 에나멜; 1.5mm; 0.25kg; max.200°C; 핵심: Cu; 포장: 16m; W 210
제조업체 부품 번호: 1030 1500 44
제조사: SYNFLEX
다음의 수량에 대한 순 가격 1 rol - 12.47 USD다음의 수량에 대한 총 가격 1 rol - 12.47 USD
다음의 수량에 대한 순 가격 3 rol - 10.91 USD다음의 수량에 대한 총 가격 3 rol - 10.91 USD
다음의 수량에 대한 순 가격 5 rol - 10.13 USD다음의 수량에 대한 총 가격 5 rol - 10.13 USD
21 TME에 재고 있음
롤 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용