+1500000 개 이상의 제품 제공
하루에 7000개의 패키지
150개국에서 28만 명 이상의 고객
게시 날짜: 20-01-2023 🕒 5 읽기 시간
If we asked random people about the abbreviation AC/DC, most of them would probably come up with the name of the legendary Australian rock band. However, the band’s name was derived from an electric device with a plate reading “AC”, which means “alternating current”. Such a short phrase would not be catchy enough for the fans, though, so the band members added the part “DC”, i.e. “direct current”. The name was meant to reflect the electrifying energy of the band’s music, and in fact it would be hard to find a more apt name for them, wouldn’t it?
Still, what’s the point of recalling a rock band’s name in a technical text? The answer is simple: the association with the iconic rock band makes it easy to remember the names of two types of electric current, which is the main subject of this text.
The concept of electric current is quite extensive. It requires delving into the physical phenomenon of the flow of positive and negative charges and the interaction of electromagnetic particles. Although seemingly complicated, it turns out to be very logical and easy to understand (at least to the elementary extent that applies to ordinary electricity users). What is electric charge and what does it have to do with electric current?
To make a long story short, electric charge is a physical feature of matter. There are two types of electric charges: positive and negative ones. According to the laws of physics, like (i.e. the same) charges repel each other while the opposite charges attract one another and tend to collide. Therefore, whenever positively charged matter meets something negatively charged, the encounter causes movement that attracts the two. When two positively or negatively charged bodies meet, they repel each other in a phenomenon called Coulomb’s force.
At his point, we reach the core of this problem – electric current is nothing else than the orderly movement of electric charges. How to initiate the movement and have it go in the direction of our choice? How to make the current appear in our electric socket? To understand the physics of electricity, let us clarify the mechanism of particle movement in conductors.
Please, note the keyword in the chapter above! A conductor is an object in which electric charges can move. It is a body full of negative charges awaiting a difference of electric potentials to move them from the higher to the lower potential. Metals are the best conductors that are commonly used for conducting electricity. The reference conductor is copper. Our everyday supply of electricity at home or work is always provided by the same channel, i.e. electric wires. Copper wires are insulated from direct contact, because they might pose a risk of electric shock to human body. Moreover, the insulation separates two phase wires from each other.
The fundamental physical quantities which describe the electric current are:
To let you see a clearer picture of that, let us compare the electric current to the flow of water. It will allow us to create a mental picture of the terms.
Let us imagine that water flowing in a pipe is equivalent to an electric current. Amperage, or current strength, is analogous to the flowing water’s speed. The faster the water flows, the higher the amperage is. Voltage is analogous to the water’s pressure. The last part of the puzzle is resistance. It may be considered as the resistance of the pipe walls, thus counteracting the water “attempting” to leak through them. Amperage and voltage are closely intertwined with each other. When the voltage changes, the amperage follows the change. Even if not perfectly synchronised, both quantities always follow each other’s changes. It is Ohm’s law that describes the relationship between these quantities with respect to electric current:
Knowing the basic formula, remember the respective units:
The fundamental difference that determines the type of electric current is the direction of its flow. Direct current flows in one constant direction while the direction of variable current may change. The most commonly used, specific type of variable current is the alternating current or AC. The direction of alternating current alternates periodically in a strictly organised manner. The number of changes per unit of time is called frequency. In all the electric sockets in the EU, the alternating current has a frequency of 50 Hz. It means that the direction of the current alternates fifty times per second. However, the current described as “variable” may change in any manner and does not have to be orderly.
Both types of electric current have distinct features, making them useful for specific solutions. Both direct and alternating currents have some advantages. Let us list the most important features of both solutions:
Let us remind you of an interesting historical fact. Two distinguished scientists of the 19th century fought with each other to prove one type of electric current better than the other. These were Thomas Edison and Nicola Tesla. They competed so vigorously that their dispute was sometimes called “a war”. Can we, however, unequivocally decide which one is better? As explained above, both direct and alternating currents have their applications, and if we eschewed any of them, we would end up very limited and devoid of many possibilities. We may only wonder what the world would be like if the pioneers of modern electrical engineering had used their time and efforts for joint research of their concepts; maybe we would be at a completely different point of technology development today...?
Transfer Multisort Elektronik (TME)은 전자 부품, 전기 기술 부품, 작업장 장비 및 산업 자동화의 세계 최대 글로벌 유통업체 중 하나입니다. 카탈로그에는 1,300개 주요 제조업체의 1,500,000개 이상의 제품이 포함되어 있습니다. Łódź와 Rzgów (폴란드)에 있는 TME의 현대적인 물류 센터는 총 면적이 40,000 m² 이상이며 매일 약 6,000개의 패키지를 150개국 이상의 고객에게 발송합니다.
TME는 또한 TME Education 프로젝트를 통해 젊은 엔지니어와 전자공학 애호가들의 지식과 기술 개발에 투자하고 있으며, TechMasterEvent 시리즈를 조직하여 혁신과 경험 교류를 촉진하면서 기술 커뮤니티를 지원합니다。