+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Capacitor is a passive component used in electrical and electronic circuits, whose primary function is to accumulate and store energy in an electrostatic field. It consists of two conductive plates separated by a dielectric - an insulating material that allows charge storage while preventing the direct flow of direct current. A capacitor’s ability to store charge is defined as its capacitance and is measured in farads.
The operating principle of a capacitor is based on the polarization of the dielectric under the influence of the electric field formed between the plates, which enables the retention of stored charges and the generation of a potential difference. Current can flow through a capacitor only during voltage changes, which makes it conductive for alternating currents while blocking direct currents in a steady state. This property is widely utilized in filters, signal component separation circuits, converters, and timing circuits.
The type of dielectric and the mechanical construction significantly affect the capacitor's characteristics, such as temperature stability, capacitance tolerance, operating voltage range, and cutoff frequency. Depending on the application, various types of capacitors are used, including ceramic, electrolytic, film, and tantalum capacitors, each with distinct performance parameters. In modern electronics, capacitors also function as filtering elements in power supplies, support reactive power compensation in power systems, and assist in the operation of memory circuits and sensors.
In pulse and high-frequency circuits, capacitors play a critical role in signal shaping and ensuring circuit stability. Their correct selection significantly influences the quality and reliability of electronic systems, whether in consumer devices, industrial applications, or telecommunications solutions.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.