+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
MOS (Metal-Oxide-Semiconductor) is a semiconductor structure forming the foundation of MOSFET transistors, widely used in modern digital and analog electronics. It consists of three layers: a thin metal layer (nowadays typically polysilicon or a high-conductivity metal), an insulating oxide layer (most commonly silicon dioxide), and a semiconductor substrate (usually n-type or p-type silicon). This configuration enables electrostatic control of current flow in the conductive region within the semiconductor without direct contact with the conducting material, allowing for miniaturization and high operational reliability.
The operating principle is based on inducing a conductive channel in the semiconductor by means of an electric field generated between the gate electrode and the substrate. When voltage is applied to the gate, charge carriers in the semiconductor are attracted or repelled in the region just below the oxide layer, leading to the formation of a conductive channel between the source and drain. The MOS structure thus enables precise current control via voltage without requiring high current in the control circuit.
MOS technology has played a crucial role in the development of integrated circuits, allowing millions of transistors to be implemented on a single chip thanks to high integration density and low power consumption. It laid the foundation for the CMOS (Complementary MOS) family, which combines p-type and n-type transistors and has come to dominate the design of digital logic circuits due to its energy efficiency and high-speed performance. The MOS structure is also used in sensors (e.g., photoelectric MOSFETs), semiconductor memories (e.g., EEPROM, Flash), and analog circuits, making it a cornerstone of modern microelectronics.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.