+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Spectrum Analyzers - definition

Spectrum Analyzers is a specialised measurement device for the representation of signals in the frequency domain, allowing a precise analysis of their harmonics and power distribution in the band. Unlike oscilloscopes, which represent signals as a function of time, spectrum Analyzers present data as a function of frequency, showing, which components of a signal have the highest energy significance in a given range.

The principle of a Spectrum Analyzer is based on the transformation of an analogue signal or digital signal to a frequency form, usually using the Fast Fourier Transform (FFT) or heterodyne circuits. This makes it possible to detect the presence of signals at specific frequencies, evaluation of electromagnetic interference, analysis of modulations, as well as testing emissions in transmitting and receiving equipment.

Spectrum Analyzers are used in a wide range of fields - from telecommunications and radiotechnics, consumer and industrial electronics, to scientific research and EMC monitoring. Thanks to their high frequency resolution and wide dynamic range, they enable the identification of signals even in the presence of strong background noise.

Devices of this type are available in both stationary, and portable versions, and their parameters - such as frequency range, analysis bandwidth, speed sampling rate or sensitivity - are selected depending on the application. Modern Spectrum Analyzers can also be integrated into computer systems, modern spectrum analysers can also be integrated with computer systems, documentation and further processing of data in a digital environment.

Spectrum Analyzers

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO