+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

BCI (brain-computer interface) - definition of

BCI (brain-computer interface). brain-computer interface) is a technology that enables direct communication between the human brain and a computer system without the intermediation of classical output channels, such as muscles or nerves. Brain-computer interfaces are designed to read the electrical signals generated by neuronal activity and convert them into commands understandable for electronic devices. The primary source of signals used in BCIs is data recorded using electroencephalographic (EEG) methods, although more advanced applications also use invasive implantation techniques.

Solutions of this type are being developed primarily in a medical context, supporting people with severe motor limitations to regain communication functions and control of their environment. In addition to therapeutic applications, BCI is the subject of intensive research in areas such as neurotechnology, human-computer interaction, robotics and augmented reality. Central to this are methods of signal processing biological signals, algorithms pattern recognition and adaptive systems that learn individual user characteristics.

BCI technologies can operate in active mode, when the user consciously initiates specific patterns of brain activity, or in passive mode, by analysing the emotional or cognitive state without directly influencing the user's decisions. Regardless of the mode of operation, the successful operation of such systems requires high-precision signal detection and immunity to endogenous and exogenous interference.

Biological complexity and the individuality of neural signals make brain-computer interfaces, make brain-computer interfaces one of the most interdisciplinary challenges of modern engineering, combining elements of neuroscience, computer science, electronics, cognitive psychology and artificial intelligence.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO