+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
A Piezoelectric Sensor is a measuring element that uses the piezoelectric phenomenon to convert mechanical pressure, vibration, force or acceleration into an electrical signal. The operation of the sensor is based on the properties of piezoelectric materials which, in response to mechanical deformation, generate an electrical charge proportional to the applied force. This phenomenon occurs in some natural crystals (e.g. quartz) and in ceramic materials produced synthetically.
In the structure of a piezoelectric sensor, the most important element is a layer of piezoelectric material, often connected to electrodes and enclosed in a suitable mechanical housing. When the material is deformed by a force, a charge shift occurs in its crystal structure, resulting in a potential difference between the electrodes. This signal can be further amplified, filtered and analysed by electronic systems.
Sensors of this type are used in applications requiring high sensitivity, a wide dynamic range and resistance to extreme environmental conditions. They are used in mechanical engineering, machine diagnostics, safety systems, medicine and consumer technology, where they are used to detect touch, vibration or pressure pulses. Due to their design, piezoelectric sensors are particularly effective in dynamic measurements, while they are less suitable for detecting static forces, as the accumulated charge is gradually dissipated.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.