+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Crystal detector - definition

The Crystal Detector is a component used in historical radio receiver systems to detect amplitude modulated signals. It works by rectifying a radio wave to extract the information contained in its envelope, the audio signal. The key component of the crystal detector is the semiconductor junction, which was originally a natural mineral such as galena (lead sulphide) bonded to a thin contact wire called a 'cat'.

The phenomenon used in the detector is based on the non-linear conduction characteristics of Semiconductors, which allows unidirectional current flow and separation of the low-frequency component from the carrier. Such a detector does not require an external power supply as it derives its energy directly from the received radio wave, making it a passive system.

Although the crystal detector has been superseded by more advanced electronics, it represents an important stage in the history of radio electronics and solid-state electronics. Its operation illustrates the basic laws of electrical engineering and the functioning of simple detection systems. Today it is used mainly for educational and experimental purposes, including the construction of simple detector receivers that do not require Batteries or other power sources. The modern equivalents of the historical crystals are solid-state germanium diodes, which provide similar rectifying properties at low threshold voltage.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO