+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Coaxial cable - definition

Coaxial Cable is a specialised transmission cable used for the transmission of high-frequency electrical signals, whose design provides excellent protection against electromagnetic interference and minimises signal loss. It consists of a central conductor, surrounded by a dielectric insulating material, which in turn is shielded by a cylindrical screen, usually made of braided copper, aluminium foil or a combination of these materials, and the whole is covered by a layer of protective outer jacket.

The central conductor is used to transmit the signal, while the screen acts as ground and an electromagnetic barrier, reducing the radiation of the signal to the outside and preventing interference from penetrating the environment. The fixed distance between the conductor and the screen and the properties of the dielectric determine the characteristic wave impedance of the cable, which in standard applications is usually 50 Ω or 75 Ω.

Coaxial cables are widely used in telecommunications systems, TV signal transmission, CCTV systems, antenna installations and in measurement and military technology. Thanks to their properties, they allow signals to be transmitted efficiently over long distances while maintaining high data integrity. In RF and microwave systems engineering, the selection of the right type of coaxial cable is crucial to ensure adequate bandwidth, minimise attenuation and impedance matching, which affects the performance of the entire transmission system.

Advanced versions of coaxial cables can be adapted to operate in extreme environmental conditions, covering a wide temperature range, UV, moisture and chemical resistance, enabling their use in industrial, aerospace and industrial applications.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO