+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Klistron is a microwave tube belonging to the class of electron tubes, used to amplify or generate signals at very high frequencies, usually in the centimeter and decimeter wave range. The principle of operation of the klystron is based on the modulation of the velocity of an electron beam, which, as a result of interactions with an array of resonators, leads to the clustering of electrons into so-called electron packets and the subsequent effective conversion of the kinetic energy of this beam into electromagnetic field energy at the desired frequency.
The basic components of a klystron are: a cathode that emits electrons, electrodes that form the beam, one or more resonators (also called modulating and output chambers), a drift space and a collector. Electrons accelerated by an electric field enter the first resonator, where their velocity is modulated under the influence of an alternating RF field. In the drift space, electrons are concentrated in the form of bursts, which induce a strong electromagnetic field when they reach the output resonator. This process can be enhanced by using further intermediate resonators.
Klistrons come in single-resonator (oscillators) and multi-resonator (amplifiers) versions, the latter being characterised by a high amplification factor and the ability to operate at high output powers. These characteristics have led to applications in radar systems, radar, satellite and television transmitters, as well as in particle accelerators and high-power transmission lines.
The efficiency of a klystron depends on the parameters of the vacuum, the geometry of the resonators, the quality of the beam focusing system and the precise tuning of the resonant frequency. Despite the development of semiconductor technology, klystrons are still indispensable for applications requiring high power and high signal stability in the microwave band.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.