+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Organic Light-Emitting Diode (OLED, Organic Light-Emitting Diode) is an advanced light source based on thin-film organic structures that emit electromagnetic radiation in the visible range as a result of recombination of charge carriers in semiconductor layers. Its operation is based on the phenomenon of electroluminescence, in which organic molecules absorb electrical energy and emit photons after electrons transition from a higher energy level to a lower excited state.
The OLED structure consists of a multilayer array of thin organic films sandwiched between two electrodes, at least one of which is transparent, allowing light emission. The emission layer, which contains organic compounds with luminescent properties, is surrounded by electron and hole transport layers that enhance charge injection efficiency and control charge recombination in the active region. The anode electrode, usually made of indium tin oxide (ITO), allows the flow of holes, while the cathode metallic, usually calcium- or magnesium-based, introduces electrons into the OLED structure.
The mechanism of operation of an OLED involves the injection of charge carriers under the influence of an applied voltage, which leads to their migration through the transport layers and recombination in the emission layer. As a result of this recombination, excitons are formed - excited electron-hole pairs which, during the relaxation process, emit photons of a specific wavelength, determining the colour of the light. Emission can occur in both the monochromatic and full-colour range in RGB matrices, where individual sub-pixels emit light in specific spectral bands.
OLED technology enables the production of displays with high contrast, wide viewing angles and fast response times, which has led to its application in TV screens, smartphones, smart watches and information panels. The flexibility of organic materials allows the creation of flexible, transparent and foldable displays, opening up the possibility of constructing a new generation of user interfaces.
Compared to conventional LEDs based on inorganic structures, OLEDs are characterised by their ability to emit their own light without the need for additional backlighting, enabling the construction of ultra-thin displays with reduced energy consumption. Advanced OLED configurations include PHOLED (Phosphorescent OLED) variants, which use phosphorescent phosphors to increase light efficiency, and WOLED (White OLED), used in lighting technology to generate white light with a wide colour spectrum.
The stability and lifetime of OLEDs depend on the quality of the organic materials and their resistance to degradation by moisture and oxygen. Advanced protective layers, encapsulation in encapsulated structures and encapsulation technologies based on gas-impermeable materials are used to increase the lifetime of the devices. Research into TADF (Thermally Activated Delayed Fluorescence) materials and new conductive polymers is leading to further optimisation of energy efficiency and improved durability of next-generation OLED displays.
In the context of industrial applications, OLED displays are finding use in active matrix technologies (AMOLED), where each pixel is individually controlled by thin-film transistors (TFTs), enabling dynamic luminance management and high image quality. The integration of OLEDs with control systems and touch sensors allows the development of interactive display surfaces, used in augmented reality and HMI (Human-Machine Interface) systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.