+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The wiring box is an electrical infrastructure component designed to protect, organise and connect electrical cables in low and medium voltage systems. It is an essential component of electrical networks in residential, industrial and commercial buildings, providing a safe and durable environment for cable connections, connectors, sockets, switches and other electrical installation equipment.
Usually made of non-combustible materials such as plastics (e.g. polycarbonate, polyamide, PVC) or metal (galvanised steel, aluminium), an electrical junction box must meet standards for mechanical resistance, waterproofing (degree of protection IP) and resistance to environmental factors such as moisture, dust or aggressive industrial atmospheres.
Depending on the type of installation, boxes are divided into surface-mounted, flush-mounted and specialised variants intended for installation in hollow-core technology, lightweight constructions or channel systems. Their design includes openings or cable grommets for the insertion and fixing of cables, as well as adequate working space for making electrical connections in accordance with the art of installation and safety rules.
Electrical junction boxes play a key role in the organisation of the distribution network, minimising the risk of mechanical damage, overheating of connections and the occurrence of short circuits, as well as allowing easy service access to system components. In modern intelligent building systems, boxes are often integrated with communication modules, lighting control systems or components of alarm and Building Automation systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.