+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Thin-film transistor (TFT) - definition

Thin Film Transistor (TFT, Thin Film Transistor) is a type of field-effect transistor (FET) with a thin film semiconductor structure, mainly used in control circuits liquid crystal display (LCD) arrays, OLED displays and other microelectronic applications requiring high-density integration and precise control pixels. Its design is based on the deposition of thin layers of active semiconductor material on a dielectric substrate, which distinguishes it from classical MOSFETs, which are fabricated in monolithic silicon structures.

The structure of a thin-film transistor includes a semiconductor layer, source (Source) and drain (Drain) electrodes, dielectric insulating layer and gate (Gate), which controls the flow of charge through the conduction channel. Semiconductor material, can be made of amorphous silicon (a-Si), polycrystalline silicon (poly-Si), organic semiconductors or metal oxides such as IGZO (Indium-Gallium-Zinc Oxide), which determines the electrical properties of the transistor, including carrier mobility and switching time.

The operation of the TFT transistor is based on modulation of the conductance in the semiconductor channel by a voltage applied to the gate, which allows precise control of the current flow between the source and drain. In liquid crystal displays, each pixel is controlled by an individual thin-film transistor, which turns on and off the voltage that polarises the liquid crystal, enabling dynamic image management and achieving high contrast and short response times.

TFT technology has found its way into modern high-resolution displays, enabling the integration of advanced active matrices (AM, Active Matrix) that provide precise control of the intensity of individual sub-pixels. Variants made from low-temperature polycrystalline silicon (LTPS, Low-Temperature Polycrystalline Silicon) have faster switching speeds and higher energy efficiency, allowing the design of thin, flexible and energy-efficient panels for use in mobile devices and augmented reality technology.

Cutting-edge developments in the field of thin-film transistors include the development of transparent technologies and flexible electronic structures, using organic Semiconductors and nanomaterials to produce ultra-thin displays with improved mechanical durability. The implementation of IGZO Transistors allows for a significant reduction in leakage currents and an improvement in the quality of displays in terms of colour reproduction and energy efficiency, with applications in medical monitors, aerospace displays and panels for industrial applications.

Integrated TFT transistors are also used in touch sensors, E-paper control systems and modern microelectronic systems, where their thin-film design allows miniaturisation and improved performance compared to conventional technology based on massive semiconductor structures.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO