+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Cold cathode is electrode emitting electrons without the need for heating, as opposed to glow cathodes, which require high temperatures to achieve thermionic emission. Emission in the case of a cold cathode is by field emission, secondary emission or emission by interaction with an ionised gas. It is most commonly encountered under conditions of electrical discharge in a gas, where a strong electric field accelerates the electrons and causes them to be released from the electrode surface.
Cold cathodes are used in many vacuum and gas devices, such as fluorescent lamps, discharge lamps, nixie indicators, ionisation manometers or X-ray sources. In modern technology they are also used in cold cathode fluorescent lamps (CCFL - Cold Cathode Fluorescent Lamp) Cold Cathode Fluorescent Lamp) and in some microscale constructions, based on carbon nanotubes and emitters of semiconductor materials.
Cold cathode design can be based on metals with low electron exit work, micro-scale blade materials, or on special coatings with electron emission properties. The key performance parameter is the value of the electric field required to initiate emission, as well as the durability of the material under ion bombardment conditions.
Cold cathodes have the advantage of immediate availability and low power consumption for emission purposes, which makes them advantageous in applications requiring quick turn-on and operation under vacuum conditions. On the other hand, their disadvantages can be their limited lifetime compared to hot cathode designs and greater sensitivity to changes in operating conditions, such as gas pressure, temperature and degree of electrode contamination. In vacuum technology and microelectronics advanced cold cathode solutions are being developed, that integrate material properties with precise emitter geometry.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.