+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Electrical discharge - definition

An electric discharge is the process of dynamic flow of electric charges through a dielectric or gas, leading to instantaneous electrical conductivity in a normally insulating medium. The phenomenon occurs when the intensity of the electric field exceeds the critical value for the medium, causing dielectric breakdown and initiation of current flow. The discharge mechanism involves the generation and acceleration of charge carriers such as electrons and ions, leading to an exponential increase in conductivity through the processes of collisional ionisation and secondary emission.

Depending on the characteristics of the current, voltage and properties of the medium, electrical discharges can take various forms, including corona, spark, arc and piercing discharges. Spark discharge, occurring in gases, is a fast, short-lived process that generates strong electromagnetic and light pulses. Arc discharge, which is stable in nature, is used in welding and plasma cutting technologies and in high-current switches.

In electrical power systems, electrical discharges are important for both utility and protection aspects. Designing insulation high voltage, lightning protection devices and surge protection requires detailed modelling of the discharge and consideration of parameters such as breakdown voltage, rise time current and radiated emission characteristics. In modern scientific research, electrical discharges are also analysed in the context of applications low-temperature plasma, gas and surface cleaning technologies, as well as in atmospheric physics experiments such as modelling lightning discharges and their effects on the Earth's electromagnetic environment.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO