+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Combinatorial system - definition

A combinational circuit is a type of digital logic circuit whose outputs depend only on the current states of the inputs, with no memory elements or history of previous signals involved. This means that, at any moment in time, the system's response is a logical function of only the current set of input signals, rather than a sequence of their changes over time. Such structures form the basis of many basic digital functions, such as binary arithmetic, decoding, multiplexing, comparison or code conversion.

Combinational circuits are built from elementary logic gates - AND, OR, NOT and their combinations - which perform defined logic functions described by Boolean equations or truth tables. Their lack of memory makes them deterministic and they respond instantaneously (ignoring propagation delays) to changes in input states. Their operation can be unambiguously determined using logic analysis, without the need to consider internal states.

In practice, combinational circuits are designed both at the level of discrete circuits, and in an integrated form using CMOS, TTL or FPGA technology. Their configuration is used in microprocessor systems, digital automation, data processing and digital interface circuits. Unlike sequential circuits, which use flip-flops and a clock to store states, combinational circuits have no timing structure and do not generate cyclic responses.

An important aspect of combinational circuit design is to minimise the number of gates and optimise latency, which affects the speed and energy efficiency of digital systems. Modern design methods use hardware description tools, such as VHDL or Verilog, which allow automatic logic synthesis based on functional design specifications.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO