+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
A Photodetector is a semiconductor or vacuum element that converts electromagnetic radiation - usually in the range of visible light, ultraviolet or infrared - into an electrical signal. Its principle of operation is based on the photoelectric effect, consisting in the generation of electric charges (electrons and holes) under the influence of an incident photon with sufficiently high energy. Depending on their design and range of operation, photodetectors are used for light intensity measurement, optical pulse detection, imaging, fibre optic communications and in Automation and security systems.
The most common types of photodetectors include Photodiodes, Phototransistors, Photoresistors and Photomultipliers. Each of these elements is characterised by different electrical properties, sensitivity, speed of response and wavelength range. Photodiodes, including PIN diodes and avalanche diodes (APDs), offer high speed and are widely used in telecommunications and medical applications. Photomultipliers, on the other hand, provide exceptional sensitivity due to cascade amplification of the signal, making them useful in single photon detection systems and experimental physics.
The characteristics of a photodetector are determined by parameters such as spectral sensitivity, time response, intrinsic noise, threshold voltage and response linearity. In advanced technical and scientific applications, the ability to operate over a wide dynamic range and resistance to environmental disturbances such as temperature or ionising radiation are also important.
Today's photodetectors can be integrated into CMOS or CCD arrays, enabling the creation of image sensors for cameras, optical sensors and vision systems. In Automation and robotics systems, they enable object detection, positioning and quality control. Their technological development includes materials such as gallium arsenide, silicon, germanium or new nanomaterial structures, which allows to extend the range of operation and increase the precision of detection.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.