+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Electric Motors - definition

Electric Motors is an electromechanical device that converts electrical energy into mechanical energy, usually in the form of torque transmitted to a shaft. The principle of operation is based on the interaction of a magnetic field with electric currents in conductors, which - according to the Lorentz force law - leads to a mechanical force. The motor design usually comprises a stationary part (stator ) in which a magnetic field is generated, and a moving part (rotor ) which starts to rotate under the influence of this field.

Electric Motors are classified according to the type of power supply into direct current (DC) motors and alternating current (AC). The AC Motors group includes asynchronous (induction) motors, synchronous and brushless motors, while DC Motors include brush and brushless (BLDC) units. Each type has unique characteristics related to construction, control and operating characteristics, which determines their use in various industrial and technical fields.

The basic parameters characterising a motor are power rating, supply voltage, speed, efficiency, torque and type of control. Motors can operate at constant or variable loads and their selection depends on application conditions such as requirements for dynamics, control precision, operating costs and reliability. Today's electric actuators often work in conjunction with inverters, converters or servo controllers, allowing full control over motion parameters.

Electric Motors are widely used in industry, transportation, automation, domestic appliances, HVAC systems, electric vehicles, robotics and many other applications where electricity needs to be converted into rotary or linear motion. Due to their high efficiency, reliability and ability to be precisely controlled, they are a key component of today's technological and energy systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO