+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Quartz clock is a device that measures the passage of time, based on a resonator made of quartz crystal, utilizing the piezoelectric effect. When voltage is applied to a properly cut crystal, mechanical vibrations with a very stable and repeatable frequency are generated. This frequency is then electronically processed to generate pulses corresponding to seconds, minutes, and hours, and also—for digital applications—to clock microprocessor circuits.
Quartz used in clocks exhibits a natural ability to oscillate within a specific frequency range, most commonly 32,768 Hz, which corresponds to a power of two and simplifies frequency division in binary circuits. The quartz oscillator, being the core of the clock, provides high precision in time measurement with minimal influence from external factors such as temperature or supply voltage. This stability is what makes quartz clocks characterized by deviations of a few seconds per month, which is highly accurate for consumer and industrial applications.
Quartz clocks can be analog, where an electric pulse controls a stepper motor driving the hands, or digital, where pulses are calculated by a logic circuit and displayed on a liquid crystal or diode screen. This technology is used in wristwatches, electronic devices, computers, automation systems, and real-time clock (RTC) applications where process synchronization with precise time reference is required.
Despite the development of more advanced synchronization technologies, such as atomic clocks or GPS systems, quartz clocks remain widely used due to their low cost, simplicity of construction, reliability, and sufficient accuracy for most everyday and industrial applications.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.