+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Bod - definition

Bod (English. baud) is a unit of measurement used in telecommunications and electronics to determine the symbol rate of data transmission in a communication channel. Means the number of signal state changes per unit of time, expressed in bauds (Bd), where one bd corresponds to one symbol change per second. Is a fundamental parameter in digital transmission systems, directly related to channel capacity, but not always equivalent to the actual number of transmitted bits per second, because a single symbol can represent more than one bit of of information.

The relationship between bod value and binary bit rate depends on the technique of modulation and the amount of information encoded in each signal state change. In transmission systems using binary keying (ASK, FSK, PSK) each state change carries exactly one bit, so the rate in baud is equal to the bit rate in bits per second (bps). In more advanced modulation methods, such as QAM (Quadrature Amplitude Modulation) or multilevel PSK, each symbol can represent multiple bits, which allows to increase the effective transmission rate while keeping the same number of signal changes.

In communication systems, bod is an important parameter for determining the bandwidth of a transmission system, because an increase in symbol rate requires an increase in bandwidth of the transmission channel. Limitations resulting from attenuation and interference in the transmission medium necessitate the use of compensation techniques, such as error correction, adaptive filtering and linear coding, which minimize the impact of distortions and reduce bandwidth requirements while maintaining high transmission quality.

In classic communication interfaces, such as serial transmission RS-232, bod value specifies the nominal data transmission rate, whereby the actual throughput also depends on the configuration of the transmission protocol, including control bits, parity and inter-frame gaps. In modern systems, such as fiber-optic transmission or wireless communication, bod is one of the parameters determining the optimization of signal coding, enabling efficient use of spectral resources and minimizing electromagnetic interference in the transmission environment.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO