+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Tachometers are measuring devices used to determine the rotational speed of a shaft or other rotating component in units of revolutions per minute (RPM) or radians per second. Its operation is based on the principle of direct or indirect measurement of the frequency of revolutions, which finds application in mechanical engineering, industrial automation systems and drive system diagnostics.
Tachometers' design includes a measuring system that converts rotational motion into an electrical, mechanical or optical signal, which is then processed to determine angular velocity values. Mechanical systems use centrifugal tachometers that use centrifugal force to control the measuring pointer or generate a voltage signal proportional to rotational speed. Electronic solutions use magnetic, optoelectronic and pulse tachometers that analyse changes in the electromagnetic field, reflections of light or the frequency of pulses generated by rotary encoders.
Modern tachometers use Hall Sensors, Inductive Sensors, speed transducers and digital signal analysis systems, allowing high measurement precision and immunity to external noise. In motor vehicles, tachometers are integrated into engine control systems to monitor crankshaft speed and optimise fuel consumption and driveline dynamics.
In industrial applications, tachometers are used in machine vibration diagnostics, machine tool spindle speed control systems CNC and torque control systems for Electric Motors. In telemetry and IoT systems they enable remote monitoring of machine operating parameters and trend analysis for predictive maintenance.
Advanced digital tachometers are equipped with communication interfaces such as Modbus, CAN or Ethernet, which enables their integration into SCADA systems and automatic control systems. Their accuracy depends on the sampling frequency of the signal, the characteristics of the transducers and noise filtering algorithms that compensate for the effects of vibration and mechanical instabilities.
In specialised applications such as aerospace, medical or robotics, tachometers operate in high speed ranges, requiring the use of laser and ultrasonic technologies that allow non-contact speed measurement in harsh environments. Their implementation in dynamic control systems enables precise management of processes requiring stable speed and synchronisation of the movement of rotating components.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.