+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Teledation - definition

Teledown is the process of remotely transmitting commands or control data to an actuator system or device located at another, often remote, location via a transmission medium. The term encompasses both the one-way transmission of information - from the operator to the controlled object - and the implementation of a feedback loop, in which the system responds to commands and provides feedback, enabling further analysis and control.

In a technical context, remote sensing is one of the key mechanisms in Automation, robotics, telemetry systems and remotely controlled devices such as drones, satellites, autonomous vehicles or robots exploration. The implementation of remote sensing requires an appropriately designed communication protocol to ensure not only the efficiency of command transmission, but also the security, noise immunity and time synchronisation of operations. The transmission medium can be wired or wireless, involving radio, fibre optic, Internet or satellite networks.

Aspects of transmission delay, link reliability and formatting of data in such a way that it can be unambiguously decoded by the receiver are important in teledata systems. Teledown can take place in manual (interactive), semi-automatic or fully automatic mode, where artificial intelligence algorithms or decision logic replace the direct actions of the operator.

The concept of teleoperation is closely related to the concepts of teleoperation and telecontrol, but refers primarily to the transmission aspect of commands rather than their physical execution or perception of the environment. In industrial and military applications, it is a key technique for the remote management of equipment in hazardous, difficult-to-access or high-precision environments.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO