+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Redox reaction - definition

Redox reaction is a chemical process involving simultaneous oxidation and reduction reactions in which electrons are exchanged between the reactants. In each redox reaction, one substance loses electrons, undergoing oxidation, while the other gains electrons, undergoing reduction. This mechanism underlies numerous chemical, electrochemical and biological processes, including corrosion of metals, combustion reactions, metabolic transformations and energy generation in electrochemical cells.

The redox phenomenon results from the difference in electrode potentials between the participating substances, which determines the direction of electron flow and the energy of the reaction. The system can be described using semi-reaction equations that illustrate oxidation and reduction processes separately, which allows the balancing of redox reactions in aqueous solutions and gaseous systems.

In the context of electrochemistry, redox reactions play a key role in the generation of electrical voltage in galvanic and electrolytic cells, where chemical transformations are used to convert chemical energy into electrical energy or vice versa. In cathode-anode systems the anode is the electrode on which the oxidation process takes place, while the cathode is responsible for the reduction. The standard potential of an electrode determines the ability of a given element or ion to donate or accept electrons, which makes it possible to predict the course of the reaction and its thermodynamics.

Redox reactions are also indispensable in materials engineering, where controlled oxidation and reduction allow the synthesis of chemical compounds with desired properties, such as anti-corrosion coatings semiconductor materials or industrial catalysts. In biochemistry, these reactions underpin the processes of cellular respiration, photosynthesis and ATP synthesis, where electrons are transported in metabolic pathways, enabling the conversion of chemical energy into forms used by living organisms.

In environmental technologies, redox reactions are used in water purification processes, reduction of gaseous pollutants and neutralisation of toxic chemicals through their controlled transformation into less reactive or inert compounds. Redox systems combined with modern electrochemical methods are used in energy storage technologies, such as flow batteries, where reversible oxidation and reduction reactions enable long-term energy storage and conversion on an industrial scale.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO