+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Haptic technology (haptics) - definition

Haptic technology, also known as haptics, is a field of engineering and human-machine interaction that deals with the generation and reception of tactile stimuli to simulate actual physical contact in a digital environment. It is based on the use of precisely controlled mechanical, electrical or ultrasonic signals, which interact with the user's skin, muscle and proprioceptive receptors to enable realistic reproduction of pressure, texture, temperature and movement sensations.

The basis of haptics are haptic actuators such as piezoelectric, electromagnetic and electrostatic actuators that generate vibrations, resistive forces or surface deformations, allowing dynamic modulation of tactile sensations. Advanced haptic systems integrate sensory feedback, allowing the intensity and characteristics of the stimuli to be adapted to the user's interaction in real time. These technologies use haptic modelling algorithms based on analysis of dynamic motion parameters, material stiffness and physical contact conditions to accurately represent interactions with virtual objects.

Virtualisation of touch finds application in human-computer interaction systems, robotics and augmented and virtual reality, where haptic feedback improves immersion and enables intuitive manipulation of digital objects. In medical applications, haptics is used in robotic surgery and training simulations, where it enables the mapping of tissue and organ resistance, increasing the precision of procedures and the safety of surgical procedures. In the industrial sector, haptic technologies are implemented in remote control and teleoperation systems, allowing robots to be manipulated in extreme or dangerous conditions.

The dynamic development of haptics includes the use of advanced smart materials, such as electroactive polymers and metamaterials with controlled stiffness, which enable adaptive changes in the properties of tactile surfaces. The use of ultrasonic and electrostatic technologies allows contact forces to be generated without direct physical contact, opening up applications in interfaces non-contact and assistive technologies. Haptic signal processing systems integrate artificial intelligence and machine learning algorithms, enabling personalisation of the tactile experience and optimisation of interactions according to individual user characteristics.

The development of haptics is supported by the standardisation of communication protocols such as APIs haptics and Tactile Internet Interfaces, which enable the transfer of tactile data over low latency networks. The implementation of haptics in IoT systems and mobile devices allows user interaction to be enriched by a realistic representation of the tactile experience, which is used in peripherals, control panels and augmented reality simulators.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO